×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 19300593, Entry date: 08/06/2004
(3)
Rate

Delivery Release for STEP 7-Micro/WIN V4.0

  • Entry
  • Associated product(s)



STEP 7-Micro/WIN V4.0 is now available.  This is the latest version of programming software for the S7-200 family of PLC's.  The price of the single license and the upgrade license will remain the same as the previous versions.  The MLFB order numbers have been changed from the previous V3.x software. 







Order No. Software
6ES7 810 2CC03 0YX0 STEP 7-Micro/WIN V4.0 Single License
6ES7 810 2CC03 0YX3 STEP 7-Micro/WIN V4.0 Upgrade License

 

Key Product Features: 

After the software is installed, you can find a 'What's New' section near the top of the Micro/WIN Project Navigation tree.  Click the 'What's New' selection for a visual overview of the product's newest features. 

  • NEW AND IMPROVED WIZARDS SUPPORT THE LATEST CPU ENHANCEMENTS 

    • PID Auto-Tune Control Panel *

    • PLC's Built-in Pulse Train Output (PTO) and Pulse Width Modulation (PWM) Position Wizard *

    • Data Logging Wizard *

    • Recipe Wizard *

  • NEW DIAGNOSTIC TOOLS

    • Online Trend Chart shows status values visually

    • Event History Log tracks the PLC's most recent events *

    • Diagnostic LED can be controlled by the PLC's program logic *

  • NEW INSTRUCTIONS AND LIBRARY ENHANCEMENTS 

    • Daylight Savings Time Instructions automate the bi-annual time switches in most all country formats *

    • Timer Tool tips and Resolution assignments visible on all Timer Instructions

    • Elapsed Time Instructions provide a way to customize timers that closely fit your application needs  *

    • Added Indirect Addressing support on more Memory Types *

    • New String Data Type (String Literals) *

    • Interrupt Clear Event Instruction *

    • Improved Support of the USS Library (for users who have previously purchased the add-on protocol instruction library)

  • NEW CPU HARDWARE SUPPORT

    • System Block gives the option for adding Program Memory instead of Run-Mode Edit *

    • System Block includes support for the new PLC onboard Analog *

    • System Block includes the extended range of the Pulse Catch Bits

  • SUPPORT FOR NEW MEMORY CARTRIDGES  

    • S7-200 Explorer Browser Tool for accessing all PLC Memory Cartridge files directly from a PC *

    • The PLC transfers now include selections for the Recipe and Data log Configurations *

    • PLC Compare includes a check of the Memory Cartridge configurations *

  • IMPROVED TD 200 AND THE TD 200C TEXT DISPLAY SUPPORT (TD 200 WIZARD)

    • New User-Defined 'Menu and Screens' Mode now available on the TD 200/C devices *

    • Multiple TD200 Language Sets can be configured in one TD configuration *

    • A Keypad Designer Tool supports the layout and creation of TD200C custom faceplates*

    • New TD200 Wizard Options to support new TD 200C features *

  • IMPROVEMENTS HELP ORGANIZE USAGE OF THE DATA BLOCKS

    • Data Block Pages, including the ability to print them individually

    • Entries into the Data Block Auto-increment to the next sequential address

  • IMPROVED USABILITY (LOOK-AND-FEEL)

    • Improved Project Tree provides direct access to all the tools, the wizard configurations, and to individual sections of the standard project components

    • ‘Define’, ‘Edit’, and ‘Select’ options for Symbols

    • Dialogs are redesigned using Selection Trees for optimized usability

    • A Project Password protects your projects from unauthorized access

    • Flexible Print of individual Wizard Configurations

* NOTES:  The * symbol is shown by the features that require the new PLC hardware. The new S7-200 PLC Hardware Delivery Release (including the new S7-200 System Manual)  is found in the Entry 19168619.

 

Compatibility:

  • STEP 7-Micro/WIN V4.0 will support all the currently offered S7-200 CPU's of the 22x series (CPU222, CPU224, CPU224XP, CPU226 and CPU226XM). 

  • All programs created with earlier versions of STEP 7-Micro/WIN can be opened with the new STEP 7-Micro/WIN Version 4.0.  The software Readme file explains special restrictions on compatibility.

  • Micro/WIN versions 3.2.x and earlier cannot open or upload version 4.0 projects.

  • Projects created with STEP 7-Micro/WIN Version 2.x or earlier must be saved in the STL editor, using the V2.x Micro/WIN, before they can be opened with STEP 7-Micro/WIN V3.x or V4.x.  For this reason, you will find the V2.1 STEP 7-Micro/WIN software in a sub-directory of your installation CD.

Operating System Support:

  • The software requires a Windows 2000/SP3 or a Windows XP (Home or Professional) operating system. 

  • The software installs in 6 languages (English, German, Italian, French, Spanish, Chinese).  

 

Your SIMATIC contact at your local Siemens office will answer any further questions you may have. 

Siemens-Partners on the Internet




Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit