Entry type: Download, Entry ID: 19440762, Entry date: 05/08/2012
(21)
Rate

New Primary Setup Tool (PST) version 4.2 and 4.1 for setting addresses of SIMATIC NET Industrial Ethernet products available as download

  • Entry
  • Associated product(s)
New Primary Setup Tool (PST) version 4.2 and 4.1 for setting addresses of SIMATIC NET Industrial Ethernet products available as download

The new Primary Setup Tool (PST) - version 4.2 is available for the Windows 8.1 (32/64-bit) operating system effective immediately.

DESCRIPTION:

Primary Setup Tool (PST)

You can use the Primary Setup Tool (PST) to assign an address (e.g. IP address) to SIMATIC NET network components, Ethernet CPs and gateways.

This is possible only when these SIMATIC NET devices have a default ETHERNET (MAC) address and can be reached online in the network.

Comment:

These settings are also possible with STEP 7 (see STEP7 documentation). In the future, you will be able to assign addresses to additional SIMATIC NET Ethernet products using the PST Tool or STEP 7. Refer to the respective product information.



Information on the PST Tool V4.2

Major innovations for the PST Tool V4.2

  • Support of these operating systems:

    • 32-bit: Windows 7 Professional/Ultimate SP 1

    Windows 8.1 Professional

    • 64-bit: Windows 7 Professional/Ultimate SP 1
      Windows Server 2008 Standard R2
      Windows 8.1 Professional

    Windows Server 2012 Standard R2

  • Filter view for more clearly structured display of modules and devices

  • New device families are supported:

    • SIMATIC RF 600

INSTALLATION

The installation program is a self-extracting ZIP file. In Windows Explorer, double-click the file or start the program with the Windows menu command Start -> Run.
A guide with information on further installation is available in the fileRegistrierung notwendig liesmich_v4p2.htm (60.2 KB)/ Registrierung notwendig readme_v4p2.htm (60.4 KB)of the PST Tool.


Download

Third-party software - License conditions and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable license conditions of such third-party software in the Readme_OSS file.

Special information for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Registrierung notwendig ReadMe_OSS.html (194.8 KB)


Download:

Registrierung notwendig pst_v4p2.zip (217.8 MB)

Additional information

Additional information on the Primary Setup Tool (installation, configuration, handling, etc.) is available in the manual:

ph_primary-setup-tool_0_v4p2.pdf (1.9 MB)

ph_primary-setup-tool_76_v4p2.pdf (3.3 MB)



Information on the PST Tool V4.1

Major innovations for the PST Tool V4.1


  • Support of these operating systems:

    • 32-bit: Windows 7 Professional/Ultimate SP 1

    Windows XP Professional SP 3

    • 64-bit: Windows 7 Professional/Ultimate SP 1
      Windows Server 2008 Standard R2

  • Filter view for more clearly structured display of modules and devices

  • New device families are supported:

    • ET 200 S CPU

    • SIMATIC S7 Embedded Controller

    • SINAMICS

    • SINUMERIK NCU

    • SIMATIC S7-1200

    • SCALANCE X500

    • MV 420/440 sensors

    • SIMOCODE pro PN switchgear

    • Sitras PRO

    • SIMOTION

INSTALLATION

The installation program is a self-extracting ZIP file. In Windows Explorer, double-click the file or start the program with the Windows menu command Start -> Run.
A guide with information on further installation is available in the fileRegistrierung notwendig liesmich_v41.htm (60.5 KB)/ Registrierung notwendig readme_v41.htm (62.9 KB).

Download

Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Readme_OSS file.

Special information for resellers

The information and the license terms in the Readme_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Registrierung notwendig ReadMe_OSS.html (194.8 KB)

Download:

Registrierung notwendig pst_v41.zip (84.9 MB)

Additional information

Additional information on the Primary Setup Tool (installation, configuration, handling, etc.) is available in the manual:

ph_primary-setup-toolv41_0.pdf (410.5 KB)

ph_primary-setup-toolv41_76.pdf (454.9 KB)


Note:

This software is provided to you free of charge, which means claims under warranty do not apply.
The "Terms of Use" at the end of this homepage also apply.
If the product package also includes open source software or other software components from third parties with specific terms of use, the software will be accompanied with information in the "Readme" file about the special conditions of the licensors that apply to this open source software or other third-party software.