×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 19440762, Entry date: 06/20/2017
(30)
Rate

New Primary Setup Tool (PST) version V4.2 HF1, 4.2 and 4.1 for setting addresses of SIMATIC NET Industrial Ethernet products available as download

  • Entry
  • Associated product(s)
New Primary Setup Tool (PST) version 4.2 HF1, 4.2 and 4.1 for setting addresses of SIMATIC NET Industrial Ethernet products available as download

Description:

New Primary Setup Tool (PST) version 4.2 HF1, 4.2 and 4.1 for setting addresses of SIMATIC NET Industrial

Ethernet products available as download.

Effective immediately, the new Primary Setup Tool (PST) - version 4.2 HF1 is available for the Windows 10 (64-bit)

operating system.


DESCRIPTION:

Primary Setup Tool (PST)

You can use the Primary Setup Tool (PST) to assign an address (e.g. IP address) to SIMATIC NET network components, Ethernet CPs

and gateways.

This is possible only when these SIMATIC NET devices have a default ETHERNET (MAC) address and can be reached online in the network.


Comment:

These settings are also possible with STEP 7 (see STEP 7 documentation). In the future,

you will be able to assign addresses to additional SIMATIC NET Ethernet products using the PST or STEP 7. Please

refer to the respective product information.


Information on the PST Tool V4.2 HF1

Major innovations for the PST Tool V4.2 HF1

  • Support of these operating systems:

    • 32-bit: Windows 7 Professional/Ultimate SP 1

Windows 8.1 Professional

    • 64-bit: Windows 7 Professional/Ultimate SP 1

Windows Server 2008 Standard R2

Windows 8.1 Professional

Windows Server 2012 Standard R2

Windows 10 Pro

Windows 10 Pro Version 1607

  • Support for new device families:

    • SCALANCE XC200

    • IE/PB Link V3


INSTALLATION

The installation program is a self-extracting ZIP file. In Windows Explorer, double-click the

file or start the program with the Windows menu command Start -> Run.

A guide with information on further installation is available in the file Registrierung notwendig liesmich_v4p2p1.htm (76.4 KB)/Registrierung notwendig readme_v4p2p1.htm (84.0 KB) of the PST Tool.


Download

Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as

applicable license conditions for this type of third-party software in the file ReadMe_OSS.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party

to avoid license infringements by the reseller or purchasing party.


Security fixes and improvements

  • Correction of SSA- 275839: Denial-of-Service Vulnerability in Industrial Products

  • Correction of SSA-701708: Local Privilege Escalation in Industrial Products


Minor security improvements

This version contains security-related improvements to increase the robustness. An update is recommended.



Download:
Registrierung notwendig PST_V4_2_0_1.zip (278.3 MB)


Additional information

Additional information on the Primary Setup Tool (installation, configuration, handling, etc.) is available

in the manual:

ph_primary-setup-tool_de_v4p2p1.pdf (624.2 KB)

ph_primary-setup-tool_en_v4p2p1.pdf (612.7 KB)



Information on the PST Tool V4.2

Major innovations for the PST Tool V4.2

  • Support of these operating systems:

    • 32-bit: Windows 7 Professional/Ultimate SP 1

Windows 8.1 Professional

    • 64-bit: Windows 7 Professional/Ultimate SP 1

Windows Server 2008 Standard R2

Windows 8.1 Professional

Windows Server 2012 Standard R2

  • Filter view for more clearly structured display of modules and devices

  • New device families are supported:

    • SIMATIC RF 600


INSTALLATION

The installation program is a self-extracting ZIP file. In Windows Explorer, double-click the

file or start the program with the Windows menu command Start -> Run.

A guide with information on further installation is available in the fileRegistrierung notwendig liesmich_v4p2.htm (60.2 KB)/ Registrierung notwendig readme_v4p2.htm (60.4 KB)of the PST Tool.



Additional information

Additional information on the Primary Setup Tool (installation, configuration, handling, etc.) is available

in the manual:

ph_primary-setup-tool_0_v4p2.pdf (1.9 MB)

ph_primary-setup-tool_76_v4p2.pdf (3.3 MB)



Major innovations for the PST Tool V4.1

  • Support of these operating systems:


    • 32-bit: Windows 7 Professional/Ultimate SP 1


Windows XP Professional SP 3

  • 64-bit: Windows 7 Professional/Ultimate SP 1

Windows Server 2008 Standard R2

  • Filter view for more clearly structured display of modules and devices

  • New device families are supported:

    • ET 200 S CPU

    • SIMATIC S7 Embedded Controller

    • SINAMICS

    • SINUMERIK NCU

    • SIMATIC S7-1200

    • SCALANCE X500

    • MV 420/440 sensors

    • SIMOCODE pro PN switchgear

    • Sitras PRO

    • SIMOTION


INSTALLATION

The installation program is a self-extracting ZIP file. In Windows Explorer, double-click the

file or start the program with the Windows menu command Start -> Run.

A guide with information on further installation is available in the file Registrierung notwendig liesmich_v41.htm (60.5 KB)/ Registrierung notwendig readme_v41.htm (62.9 KB).


Download

Third-party software - license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as

applicable license conditions for this type of third-party software in the file ReadMe_OSS.

Special note for resellers

The information and the license conditions in the Readme_OSS file must be passed on to the purchasing party

to avoid license infringements by the reseller or purchasing party.

Registrierung notwendig ReadMe_OSS.html (194.8 KB)


Download:

Registrierung notwendig pst_v41.zip (84.9 MB)


Additional information

Additional information on the Primary Setup Tool (installation, configuration, handling, etc.) is available

in the manual:

ph_primary-setup-toolv41_0.pdf (410.5 KB)

ph_primary-setup-toolv41_76.pdf (454.9 KB)


Note:

This software is provided to you free of charge, which means claims under warranty do not apply.

Otherwise the "Terms of Use" at the bottom of this home page apply.

In case the scope of delivery of the Open Source software or other software components from third parties should include

specific terms of use, the software comes with a note in the "Readme" file

describing which special conditions of the licensers apply to this Open Source software or other

third-party software.