Entry type: Download, Entry ID: 19440762, Entry date: 05/08/2012
(6)
Rate

New Primary Setup Tool (PST) Version 4.2, plus Version V3.2, V4.0 and V4.1 for address setting of SIMATIC NET Industrial Ethernet products available for download

  • Entry
  • Associated product(s)

The new Primary Setup Tool (PST) version 4.2 for Windows 8.1 (32/64 Bit) is now available.

 

DESCRIPTION:

Primary Setup Tools (PST)

The Primary Setup Tool (PST) enables you to make address allocations (e.g. IP address) for  SIMATIC NET network components, Ethernet CPs and Gateways 

The precondition is that these SIMATIC NET devices have a preset ETHERNET (MAC) address and are accessible on-line in the network.  

Remark:

The address setting can also be done with STEP 7 (see STEP7 documentation). In the near future it will be possible to perform more address settings for SIMATIC NET Ethernet products via PST Tool and STEP 7. Please note the relevant product information.

 

 

 

PST V4.2

 

PST V4.1

 

PST V4.0

   

PST V3.2

 

 

 

 

Information on the PST Tool V4.2

 

           New features of the PST Tool V4.2

  • Support of the operating systems:
    • 32 Bit: Windows 7 Professional/Ultimate SP 1

                         Windows 8.1 Professional/Ultimate

    • 64 Bit: Windows 7 Professional/Ultimate SP 1
                 Windows Server 2008 Standard R2
                 Windows 8.1 Professional/Ultimate

                         Windows Server 2012 Standard R2

  • Filter view for the clearer representation of modules and devices
  • Support of new device families:
    • SIMATIC RF 600

         

INSTALLATION

 

The installation program is a self-extracting ZIP archive. Double-click on the file in the Windows Explorer or execute the program via the Windows command Start -> Execute.
Please also read the installation instructions in the filesliesmich ( 60 KB ) /Readme ( 60 KB ) of the PST Tool.

 

 

Download

 

PST-Tool_V4.2 ( 223063 KB )

 

 

            

More information

More information on the Primary Setup Tool (installation, configuration, handling, etc.) is available from the Handbuch ( 1990 KB ) / Manual ( 3426 KB ) .

 

 

 

 

Information on the PST Tool V4.1

 

           New features of the PST Tool V4.1

  • Support of the operating systems:
    • 32 Bit: Windows 7 Professional/Ultimate SP 1

                         Windows XP Professional SP 3

    • 64 Bit: Windows 7 Professional/Ultimate SP 1
                 Windows Server 2008 Standard R2
  • Filter view for clearer representation of modules and devices
  • Support of new device families:
    • ET 200 S CPU
    • SIMATIC S7 Embedded Controller
    • SINAMICS
    • SINUMERIK NCU
    • SIMATIC S7-1200
    • SCALANCE X500
    • Sensors MV 420/440
    • SIMOCODE pro PN switching devices
    • Sitras PRO
    • SIMOTION

         

INSTALLATION

 

The installation program is a self-extracting ZIP archive. Double-click on the file in the Windows Explorer or execute the program via the Windows command Start -> Execute.
Please also read the installation instructions in the files liesmich ( 60 KB ) /Readme ( 62 KB ) of the PST Tool.

 

 

Download

 

PST-Tool_V4.1 ( 86978 KB )

 

 

 

More information

More information on the Primary Setup Tool (installation, configuration, handling, etc.) is available from the Handbuch ( 410 KB ) / Manual ( 454 KB ) .

 

 

 

 

 

Information on the PST Tool V4.0

 

           New features of the PST Tool V4.0

  • Support of the 32-bit Windows Vista Ultimate/Business operating system with SP 1 and Windows XP Professional SP 2 or SP 3
  • Support of new modules and devices
  • Filter view for clearer representation of modules and devices

         

INSTALLATION

 

The installation program is a self-extracting ZIP archive. Double-click on the file in the Windows Explorer or execute the program via the Windows command Start -> Execute.
Please also read the installation instructions in the files liesmich ( 27 KB ) /Readme ( 31 KB ) of the PST Tool.

 

 

Download

 

PST-Tool_V4.0.zip ( 13315 KB )

 

 

             

More information

More information on the Primary Setup Tool (installation, configuration, handling, etc.) is available from the Handbuch ( 331 KB ) / Manual ( 321 KB ) , or the SCALANCE X/W configuration manuals, or the "SIMATIC NET Industrial Ethernet Electrical Lean Switch" manual, chapter 6.2.2 (entry ID: 13471140).

 

 

 

 

 

Information on the PST Tool V3.2

 

List of modules

The following modules permit address setting by means of the PST Tool:  

SIMATIC NET CPs:

Type Article Number further information
CP343-1 6GK7343-1GX20-0XE0 see entry ID 15392964
  6GK7343-1EX20-0XE0  
CP343-1 Lean 6GK7343-1CX00-0XE0  
CP443-1 6GK7443-1EX11-0XE0  
CP443-1 Advanced 6GK7443-1EX40-0XE0  

 

Please note:

It is important that you select "Set IP address to another path" in STEP7 HW Configuration as the source in the features dialog of the module. If connections (S7, S5 compatible connections, etc.) have been configured via the CPs by means of the STEP7 NETPRO tool, these connections will be deleted by the PST in the case of an IP address change.

 

SIMATIC NET INC (Industrial Network Components)

The following SIMATIC NET switches permit address setting by means of the PST Tool. 

 

Type Article Number further information
OSM / ESM   Function is supported with firmware version 2.3.0 and higher, see entry ID  14198951 "OSM / ESM firmware update version 2.3.0" dated 09.01.2003.

(also possible with PST V2.0 , see entry ID 14929629

ELS TP40 M 6GK1102-6AB00 see entry ID 14040243

(also possible with PST V2.0 , see entry ID 14929629  

SCALANCE W788-1PRO 6GK5788-1ST00-2AA6

6GK5788-1ST00-2AB6

For more details please see Product Information / user manual. . 
SCALANCE W788-2PRO 6GK5788-2ST00-2AA6

6GK5788-2ST00-2AB6

For more details please see Product Information / user manual.  
SCALANCE W744-1PRO (Ethernet Client Module)  6GK5744-1ST00-2AA6

6GK5744-1ST00-2AB6

For more details please see Product Information / user manual.  
SCALANCE X200 in preparation For more details please see Product Information / user manual. . 
SCALANCE X400 in preparation For more details please see Product Information / user manual.  

 

Please note:

The PST only supports SIMATIC NET network components with management functionality (Web-based management and/or SNMP). These components additionally permit calling the WEB Based Management from the PST for the purpose of diagnostics and configuration.

 

SIMATIC NET Gateways

The following SIMATIC NET gateways permit address setting by means of the PST.

Type Article Number further information
IE/PB-Link 6GK1411-5AA00

6GK1411-5AA20

see entry ID 13472319 "Delivery release of firmware V1.3.23 for SIMATIC NET IE/PB Link (6GK1411-5AA00)"
IE/PB-Link PN IO 6GK1411-5AB00 see entry ID 19310075

Please note:

The IE/PB Link additionally permits setting of PROFIBUS parameters (address, profile, baud rate).

 

INSTALLATION

Please ensure that no older version of the Primary Setup Tool is installed on your PC. If necessary, uninstall the older version first.

Please proceed as follows:

Double click the file setup.exe or select the menu command File -> Execute and specify the path to setup.exe.

The required files will be copied to the selected directory.

The DCP (Discovery and Basic Configuration Protocol) will be installed. The DLC (Data Link Control) protocol must be installed thereafter.

 

Supported operating systems

The Primary Setup Tool can be installed and executed under the following operating systems.

-Windows 2000 Professional SP2

-Windows XP Professional

Please note: Windows NT is only supported by PST V2.0, see entry ID 14929629

The installation program is a self-extracting ZIP archive. Double click the file in the Windows Explorer or execute the program via the Windows command Start -> Execute.
You will find further installation instructions in the readme file liesmich.rtf.

 

PST-Tool_V3.2.zip ( 8396 KB )

 

Installing the DLC protocol (relevant for PST version 3.2 and version 4.0)

Please proceed as follows:

- Start with the Windows command Start -> Settings -> Control panel

- Open the icon "Network connections";

- From the list of network cards select the one for which the DLC protocol is to be installed;

- Use the right-hand mouse button to open "Features";

- Press the "Install" button and select "Protocol";

- Press the "Add" button and select "Data carrier“;

- Enter the path to the sub-directory "DLC Protocol“ in your Primary Setup Tool installation folder and click "OK“;

- Confirm the selection of the DLC protocol with OK;

 

You can uninstall the software via Start->Settings->Control panel->Software->Primary Setup Tool. The DCP protocol is also uninstalled in this case.

The DLC protocol is not uninstalled when you uninstall the PST. To remove the DLC protocol you must uninstall it separately: first open the features page of the network card, select "DLC Protocol" and press the "Uninstall" button.

 

 

 

 

 

Please note:

This software is available to you free of charge, claims on the warranty of defects will not be accepted.
Otherwise, the "Terms of Use" cited at the end of this homepage are applicable.
In the event that the scope of delivery includes Open Source Software or other software components of third parties with specific conditions of use, the software will include a note in the "Readme" file to indicate which special conditions of the licensee are applicable to this Open Source Software or non-Siemens software.