×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 19514638, Entry date: 06/02/2005
(1)
Rate

How do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client?

  • Entry
  • Associated product(s)


Instructions:

Software requirements:

  • S7-200 PC Access OPC Server V1.0.0.56
  • WinCC flexible 2004 Advanced
  • WinCC flexible 2004 Runtime

Hardware requirements:

  • S7-200 communications cable
  • S7-22x CPU
  • PC

A further requirement is that a properly functioning STEP 7 Micro/WIN project is available and loaded into S7-200 CPU.

Configuring the OPC server with S7-200 PC Access

  • Start S7-200 PC Access via Start > SIMATIC > S7-200 PC Access V1.0.0.56 > S7-200 PC Access.
  • Create a new project.


Fig. 01
  • Mark controller, e.g. "MicroWIN (CP5611(PPI))", and open the dialog Status > PG/PC Interface....
  • As access point of the application you must set "Micro/WIN" with the existing communications connection to the S7-200, e.g. "-->CP5611(PPI)".

Note:
If the access point is not "Micro/WIN", first close the dialog and set the access point via Control Panel > Set PG/PC Interface.

  • Close the dialog via OK.


Fig. 02
  • Via File > Import Symbols you import the symbol of the selected STEP 7 Micro/WIN project.
  • Then save the configuration you have created.
  • In S7-200 PC Access you can now access the symbol of the STEP 7 Micro/WIN project.


Fig. 03
  • If you mark the project folder "Project1", for example, you can check the address of the PLC via Edit > Properties.


Fig. 04

Checking the connection with Test OPC Client of S7-200 PC Access

  • Mark the symbols in the right-hand project pane of S7-200 PC Access.
  • Using drag and drop add the marked variables as items to Test Client (bottom project pane).


Fig. 05
  • Enable Test Client via Status > Start Test Client.
  • If "Good" is displayed for Quality, the variable has been read successfully out of the S7-200 controller.


Fig. 06

WinCC flexible Runtime as OPC client

  • Start WinCC flexible 2004 Advanced.
  • Create a WinCC flexible project for a PC via PC > WinCC flexible RT.
  • In the project tree double-click on Communication > Connections to create a new connection.
  • As communications driver for the connection select OPC.
  • Select "S7200.OPCServer" for OPC server.

Note:
If the S7-200 OPC server has not been started on the local PC, you must specify the computer name or the IP address of the remote PC on which the S7-200 OPC server is located. When accessing the OPC server via network, please refer to the DCOM settings in the WinCC flexible Online Help under "Communication > OPC > Commissioning the OPC > DCOM".


Fig. 07
  • Add a variable under Communication > Variables.
  • Via Symbol you select the relevant item of the S7-200 OPC server.


Fig. 08
  • You can display this variable via an input/output field in the Start picture.
  • Save the configuration.
  • Start WinCC flexible Runtime via the icon in the toolbar.


Fig. 09
 


Fig. 10

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.