Entry type: FAQ, Entry ID: 19548096, Entry date: 10/05/2004
(0)
Rate

Using C-PLUG with network components and SIMATIC CPs

  • Entry
  • Associated product(s)


QUESTION:
 
What function does the C-PLUG have with network components and SIMATIC Cps ?

ANSWER:  
The C-PLUG is a removable medium that supports rapid device change without having to configure the replacement device if there is a fault. All you do is remove the C-PLUG from the failed device and insert it in the replacement device. The replacement device then starts up automatically with the same configuration as the failed device.

The C-PLUG can usually be used as an option, in other words the devices can also be operated without C-PLUG.

In the case of some S7 CP modules, such as the CP 443-1 Advanced, the C-PLUG is part of the delivery package and is required for the complete scope of functions of the components concerned


Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster