×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 19701610, Entry date: 12/28/2017
(21)
Rate

How do you do an operating system update on operator panels or perform a "Reset to factory settings"?

  • Entry
  • Associated product(s)
Below we provide you with an overview of when you must update an operating system and how to do the update depending on the software used.

Explanation of terms "Operating System Update" and "Reset to factory settings"
With an operating system update you delete the following data on an operator panel:

  • WinCC (TIA Portal) or WinCC flexible configurations
  • User administration
  • Recipes

When you do a reset to factory settings you also delete:

  • Licenses

Before making an update or reset you should correspondingly make a backup of this data using ProSave and the ALM.
You should do a reset to factory settings by preference for repairing operator panels with damaged operating systems that are otherwise no longer operable.

Procedure
The following documents provide instructions for operating system updates and resetting to factory settings depending on the configuration software and the operator panels being used.

  1. "Operating System Update" and "Reset to Factory Settings" with
    WinCC (TIA Portal)

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the WinCC (TIA Portal) software.

Note
With WinCC V11 and higher you no longer need an operating system update in the different versions (for example, WinCC V11 SP1, WinCC V11 SP2, etc.). When you transfer a project, all the currently associated system files (DLLs) are also transferred automatically to the operator panel. The Basic Panels are the exception here.

Attachment 1: WinCC_TIA_Portal.pdf ( 489 KB )

Contents
1 Operating System Update with WinCC (TIA Portal)
     1.1 Operating System Update (OS Update)
     1.2 Reset Operator Panel to Factory Settings (Booting)
          1.2.1 Operator Panel with Defective Operating System
          1.2.2 Operator Panel with Intact Operating System
2 Further Information
     2.1 Cable Connection between PC and Operator Panel
          2.1.1 Operating System Update
          2.1.2 Reset Operator Panel to Factory Settings (Booting)
     2.2 Set Image Path / File in ProSave
          2.2.1 Image Path in WinCC (TIA Portal)
          2.2.2 Image Path in WinCC flexible 2008
     2.3 Determine MAC Address
3 Problem Analysis
     3.1 Disconnection of RS232/PPI Multi Master Cable
     3.2 Check Box Cannot be Selected in ProSave
     3.3 Check Box Cannot be Deselected in ProSave
     3.4 Error Message when Transferring the Configuration
     3.5 Connection to Operator Panel Cannot be Established
          3.5.1 Check Transfer Type and Address on the Operator Panel
          3.5.2 Check Cable Connection and Connectors
          3.5.3 Check PG/PC Interface on the Configuration Computer.


  1. "Reset to factory settings" with WinCC (TIA Portal) and Basic Panels 2nd Generation
    To reset Basic Panels 2nd Generation (KTP400 Basic, KTP700 Basic / KTP700 Basic DP, KTP900 Basic, KTP1200 Basic / KTP1200 Basic DP) to factory settings you use a USB memory stick that you you have prepared with the corresponding USB Recovery Software as described in Entry ID 109744950.

  2. "Operating system update" or "Reset to factory settings" with WinCC flexible

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the WinCC flexible software.

Attachment 2: WinCC_flexible.pdf (784 KB)     

4. "Operating System Update" and "Reset to Factory Settings" with ProSave (Stand alone)

The PDF document includes instructions for how to do an "Operating system update" or "Reset to factory settings" (booting) using the ProSave software.

  19701610_prosave_1_2_e.pdf (1,1 MB)

System Events
The following table gives an excerpt of possible system events when the configuration is to be transferred to the operator panel and the operating system version of the operator panel does not match the installed Engineering Software.
 

No image found. Waiting for image update…,
Incorrect operating system version on the operator panel. Update the operating system? (0800:000011)
Downloading is not possible. The "version of the device" in your WinCC flexible project and the version of the operating system of the device are not compatible. Do you want to update the operating system of the HMI device?
Transfer is not possible. The "version of the operator panel" in your WinCC flexible project and the version of the operating system of the operator panel are not compatible. Please perform an operating system update for the operator panel with the command "Project > Transfer > OS Update" ("Reset to factory settings" if necessary).
Table 01

Further Information
More information on this topic is available in the following entries:
 

How do you do a "Reset to factory settings" on an MP 377 operator panel?35677293
What connections are there between the version designations in WinCC flexible?21742389
Which version of Image of the relevant operator panels can be used for the corresponding version of ProTool?28263711
What is the serial cable assignment for transferring the configuration to a Windows-based device?21401061
Which components do you use to terminate PROFIBUS subnets with a terminator?187276
Table 02

Additional Keywords
OS Update, Operating system, Boot, Boot Loader, Transfer settings, RS232/PPI multimaster cable, Freeport, PPI, USB, Boot settings, Reboot, Basic, Comfort, Advanced, Professional, Panel Factory Settings, Panel Overall Reset, Panel Reset

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit