×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 19952049, Entry date: 11/30/2004
(0)
Rate

Substitute for closed-loop control module IP252

  • Entry
  • Associated product(s)

QUESTION:  
Can the closed-loop control module, order number 6ES5252-3AA21, be substituted by closed-loop control module 6ES5252-3AA13? 
What is the difference between the two modules?

ANSWER:  
Closed-loop control module 6ES5252-3AA21 is a special version of the IP252 modules with a special firmware for the 12MHz applications and cannot be substituted by closed-loop control module 6ES5252-3AA13. 
Module 6ES5252-3AA21 does not have the drive and standard closed-loop controller structure of module 6ES5252-3AA13 and was developed specially for fast closed-loop controller tasks in synthetic materials technology and for hydraulic drives.

Module 6ES5252-3AA21 can still be ordered as a replacement module at:

http://www.siemens.de/automation/migration-support

Keywords:
REWA 00029 R1


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit