×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 20012938, Entry date: 12/13/2013
(0)
Rate

Which memory modules can you program with the SIMATIC USB prommer?

  • Entry
  • Associated product(s)

Instructions
With the SIMATIC USB prommer (order number: 6ES7792-0AA00-0XA0) you can only program the micro memory cards (order number: 6ES7953-...) required for the FM458-1DP. It is not possible to program the following memory modules offline using a D7-SYS program:
 

Memory module Description Order number
MS5 Program memory module 
2MB
6DD1610-0AH0
MS51 Program memory module 
4MB
6DD1610-0AK0
MS52 Program memory module 
8MB
6DD1610-0AH2
MC500 Program memory module for FM458 
4MB
6DD1610-0AH4
MC510 Program memory module for SIMATIC TDC 
8MB
6DD1610-0AH6
MC521 Program memory module for FM458 
2MB
6DD1610-0AH3

Note
You can program these MS... memory modules in a PG or PC with a USB interface through the "OmniDrive USB LF" which you must connect externally. More information about this is available in Entry ID: 17624774.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.