×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 2008363, Entry date: 11/30/2015
(3)
Rate

What should you pay attention to when using WinCC within a domain?

  • Entry
  • Associated product(s)
You must meet specific requirements for both the installation and the operation of WinCC.

If you operate WinCC in a domain environment, refer to the notes in the WinCC manual "WinCC V7.3: General Information and Installation" in Entry ID: 109736216. The chapters "WinCC Installation Notes" and "WinCC Release Notes" provide detailed information about operating WinCC in a domain.
Pay particular attention to the chapter entitled
Software Requirements for Installation.

The diverse conditions and configurations of different plants mean that the behavior based on domain settings cannot be checked with a general system test.
Therefore it is not possible to make any concrete statements about the restrictions and effects of the many individual domain settings.

If you are still working with an old version of WinCC (< V7.3) and therefore with the operating system Windows NT, please note the information below.

Description
It is necessary to install WinCC in a local "domain user profile". If there are network problems you can log in with your local user profile and continue working with WinCC without the errors named (see Release Notes WinCC V5.0).

Note

If you install WinCC with a local profile, it can be operated both in a network environment and locally (without network).
Also make sure that there is always a configured network card in your computer. This is a requirement regardless of whether or not you want to use the network.

Procedure

  1. Create a local user profile (without network connection) with administrator rights and power user rights in addition to the existing user profiles.
    (Note: You need administrator rights yourself to be able to create a new user with administrator rights).
  • Select "Start > Programs > Management (general) > User Manager".
  • In the User Manager you select "User > New User".
       

Fig. 01
   
  1. Restart your PC.
  2. In the logon window you change the domain name to your computer name.
  3. Now log on to your computer with the newly created profile.
  4. Install WinCC.

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
ProductSupport.EntityResultListTitle
ProductSupport.EntityResultListDescription

ProductSupport.EntityResultListButtonText
Copy URL
mySupport Cockpit
Related links