×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 20614217, Entry date: 03/16/2015
(1)
Rate

Buffering of Process Messages including Time Stamps with ALARM_7B

  • Entry
  • Associated product(s)
In the case of a disrupted connection to the operator station, the process messages can be buffered by using the SIMATIC PCS 7 alarm block “ALARM_7B”. After restoration of the connection, the buffered alarms will be sent to the OS, together with the time stamp generated when the event occurred.

Task
The conventional alarm blocks "Alarm_8" and "Alarm_8P" are used to signal status changes of events/alarms to the operator system, together with a time stamp. This time stamp is generated when the alarm block is called.
For the purpose of traceability, the process messages in the automation system shall remain available, even if the connection to the operator system fails. Furthermore, a time stamp indicating the time of occurrence shall be stored and displayed when the event is displayed on the operator system at a later point.
 


Fig. 01

 

Specific projects require the transmission of alarms and messages to the operator system via a central S7-400 controller, including the original time stamps generated in subordinate systems.
This may be reasonable in configurations like the following ones:
  • In hierarchical control topologies with S7-300 controllers
  • For signal time stamping in an ET 200 unit
  • In telecontrol applications

Solution
With the solution described here, the connection between automation system (AS) and operator system (OS) can be continuously monitored. If the connection to the OS is interrupted, the alarm signals including the relevant time stamps of the events will be stored. These time stamps can be generated on the basis of the CPU clock or by an external source.
After restoration of the connection, the buffered alarms will be sent to the OS, together with the time stamp generated when the event occurred.
 
 
Fig. 02

This solution comprises the alarm block “ALARM_7B”, a documentation describing its function principle and an instruction with an example on how the block is used.

Validity

  • as of PCS 7 V7.1
  • or as of STEP 7 V5.4 SP4, S7-SCL V5.3 SP5 and WinCC 7.0 SP1

Documentation
  Buffering of Process Messages including Time Stamps with ALARM_7B (4,6 MB)

Code
 Registrierung notwendig  S7 library and PCS 7 demo project (87,4 MB)

Additional Keywords
27201952

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.