×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 21061963, Entry date: 03/29/2005
(0)
Rate

Micro Automation: Controlled Positioning of an Axis with Stepper Motor Using the Example of a "Cutting-to-Length" Process incl. HMI Configuration (MAE 10)

  • Entry
  • Associated product(s)

Problem 
The application is predestined for solving feed motion positioning tasks. Application areas are for example, feed units, material transport, paper and cardboard processing machines.

Solution
The process works as follows: An S7-200 CPU controls a stepper motor via the modules EM 253 POSITION and FM STEPDRIVE. The FM STEPDRIVE is the power unit for the stepper motor. Position and motion of the stepper motor are defined by the S7-200 CPU. The EM253 "POSITION" module transforms these values into pulses (steps) which are then converted into current values for the stepper motor rotation. The configuration can be operated and monitored via the TD200.

The build up of this application is illustrated in the following figure below.

Downloads

Content of Downloads

Download

Description (German) 
21061963_mae10_gest_pos_schritt_DOKU_v00_d.pdf ( 1878 KB )
Description (English) 
21061963_mae10_gest_pos_schritt_DOKU_v00_e.pdf ( 1801 KB )
STEP7-Micro/Win-Code
21061963_mae10_gest_pos_schritt_CODE_v00.zip ( 41 KB )
Calculation of the acceleration time
21061963_mae10_gest_pos_schritt_TAB_v00.zip ( 784 KB )

 

History

Version

Modification

03/2003 First edition