Micro Automation: Simplest possible access to PLC data via standard PC applications (MAS 11)
-
Entry
-
Associated product(s)
Note
The SIMATIC S7-200 components used in this application example are currently phased out.
This application can be realized even more effective and easier with the new SIMATIC S7-1200.
The respective application example with SIMATIC S7-1200 is available under entry-ID: 40603943, 67295801
Furthermore, many useful applications with SIMATIC S7-1200 are available under entry-ID: 35923253
Automation task
The configuration described in the set is suitable for the following tasks:
Acquisition and evaluation of process data of an S7-200 CPU on the PC
The configuration can e.g. be used for the following applications:
Archiving process data, creating statistics, operator control and monitoring of process data
Automation solution
The configuration consists of the following automation components:
CPU S7-224, PC/PG with OPC server S7-200 PC-Access and MS Excel
The software example on the configuration has the following functionality:
Reading and writing process data of an S7-200 CPU using MS Excel
Startup Code
For the startup we offer you software examples with test code and test parameters as download. The software examples support you during the first steps and tests with your Micro Automation Sets. They enable quick testing of the hardware and software interfaces between the products described in the Micro Automation Sets.
Downloads
Links
Link contents |
Link |
S7-200 system manual |
System manual |
S7-200 PC Access online-help |
Online-help |
History
Excessive of the tread "Applications & Tools"
To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.
- German
- Spanish
- French
- Italian
- Chinese
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC PLC Basic Controller S7-200 CPUs
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC PLC Basic Controller S7-200 Software S7-200 PC Access
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC Software for SIMATIC Controller STEP 7 V5.x STEP7 basic software and editors STEP 7 - Micro / WIN
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry