×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21169761, Entry date: 07/22/2015
(0)
Rate

Which versions of WinAC (Basis, RTX, Slot) and SIMATIC NET are compatible with each other?

  • Entry
  • Associated product(s)
The Compatibility Tool is a function provided by the Industry Online Support with which you can select compatible software products or check the compatibility of existing configurations.

Compatibility information for WinAC RTX V4.0 and higher and SIMATIC NET is available in the Compatibility Tool.
You can call the Compatibility Tool in the following entry.
64847781

Please use the new entry for your favorites.

You will find the following information in this entry:

  • New compatibility information
  • New Compatibility Tool functions
  • Operating instructions and Help for the Compatibility Tool

The compatibility of the older versions WinAC Basis and WinAC Slot is given in the two tables below.

Compatibility between WinAC Basis and SIMATIC NET
 

WinAC Basis SIMATIC NET
V4.0 For Windows 2000: V6.0 (SP 5 or higher)
For Windows XP: V6.1
V4.0 SP1 V6.1 SP1
V4.1 V6.2
Table 1: WinAC Basis and SIMATIC NET

Compatibility of WinAC Slot and SIMATIC NET
 

WinAC Slot SIMATIC NET
V3.2 V6.0 SP5
V3.3 For Windows 2000: V6.0 (SP 5 or higher)
For Windows XP: V6.1
V3.4 V6.2
V4.0 V6.3
Table 2: WinAC Slot and SIMATIC NET

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.