×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 21178141, Entry date: 07/16/2013
(0)
Rate

Establishing the DP response time, HMI update time and the HMI operating time for typical configurations on the non-synchronized PROFIBUS DP

  • Entry
  • Associated product(s)

Task
Many applications require a quick response time via the distributed inputs and outputs. In SIMATIC, mainly PROFIBUS DP is used for quick and efficient data exchange between distributed I/O and S7 stations. Typical DP configurations consist of a DP master and several DP slaves on a DP line. Programming devices or operator panels (load at the subnet) are often operated on the same DP line.
When planning such configurations the following questions arise even in the concept phase:

  • How long does it take until a distributed output responds to a distributed input?
  • How long does it take during process alarms until a distributed output responds to a distributed input?
  • What fluctuations can occur?
  • What influence does communication via PROFIBUS DP have on the cycle time of the DP master?
  • What times are to be expected when operating TouchPanels?

With the use of Panel PCs, some further questions arise:

  • How do the response times behave, if a WinAC RTX as well as a WinCC flexible runtime configuration run on a PanelPC?
  • What are the effects of a WinCC flexible Runtime configuration of a PanelPC on the times of additional TouchPanels?

The following screen shows the schematic layout of the measurement on a variant:

Solution
To answer the above questions, Industry Automation and Customer Services carried out extensive measurements on typical configurations with SIMATIC components, which provide planning certainty for your plants: 

  • Different DP masters communicate with up to 60 DP slaves.
  • Optionally one programming device or up to 10 operator panels are operated at the same DP line.
  • The DP Master runs with various typical user programs. Various typical configurations are loaded in the operating devices. In the programming device, the State function is active.
  • The WinAC RTX and WinCC flexible Runtime configurations are simultaneously operated on a PanelPC.

A simple user interface of a web application provides you with the results of the measurements.

Overview of the measured variables:

Measured variable

Description

DP response time (OB1) Time from receiving a process signal at the input of the ET200 until activation of an output at the ET200 (via process image).
DP response time (OB40) Time from receiving a process signal at the input of the ET200 until the activation of an output at the ET200 (via process-alarm and direct commands).
Cycle time Time between two process image transfers in the DP Master.
HMI update time Time from receiving a process signal at the input of the ET200 until the display of a color change in the TouchPanel.
HMI operating time Time from pressing an operator button at the panel until setting a process signal at the output of the ET200.
PPC update time Time from receiving a process signal at the input of the ET200 until the display of a color change in the PanelPC.
PPC operating time Time from pressing an operator button at the PanelPC until setting a process signal at the output of ET200.

Note
Measurement was performed for some typical configurations. This does not mean that every possible configuration has been measured.

Outputs on the User Interface
You can enter the desired configuration quickly and easily with an interactive user interface. The corresponding performance data is available immediately in the output table.

Access to the performance data
Click the respective version to go to the web interface of the performance data.

Version Measuring time Components used Link
V 5.0 Dec 2012 Components_List_ID28.pdf ( 12 KB ) DP_ReaV5
V 4.1 Oct 2010 Components_List_ID17.pdf ( 172 KB )

DP_ReaV4

V 4.0 Feb 2009
V 3.0 July 2008 Components_List_ID13.pdf ( 166 KB ) DP_ReaV3
V 2.0 2005 Measured_Components_of_DP_ID2.pdf ( 43 KB )

DP_ReaV2

Last modification
Update of all Component Firmware, Integration of S7-1200 systems and Comfort Panels

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.