×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21184132, Entry date: 10/21/2015
(2)
Rate

How do you send short text messages (SMS) from a WinCC (TIA Portal) or SIMATIC WinCC flexible HMI station to a mobile phone?

  • Entry
  • Associated product(s)
With WinCC (TIA Portal) and WinCC flexible it is possible to send e-mails as short text messages (SMS) to a mobile phone. The conversion into a short text message is done by the mobile network operator or your own SMTP server.

1. Configuration of mail dispatch with a SIMATIC HMI station

  • With WinCC (TIA Portal)
    The sample application 106226404 explains the configuration of the e-mail dispatch function of Comfort Panels with WinCC (TIA Portal).
  • With WinCC flexible
    Follow the instructions given in Entry18984102 to configure an e-mail message system with WinCC flexible.

2. Options for forwarding as short text message (SMS)
You have the following options for receiving e-mail messages as SMSs on a mobile phone:

  • External providers make it possible to convert e-mails into SMS messages for mobile telephones and pagers. (This option is described here.)
  • Your own SMTP server supports forwarding of e-mails via SMS message to a mobile phone or pager.

Note
The e-mail function in WinCC flexible requires the "Sm@rtService" license key.

You can send e-mails with the following panels:

  • All operator panels as from the 170 series with Ethernet interface except Basic Panels
  • PCs with WinCC flexible Runtime and Ethernet interface

3. Enabling and disabling SMS messaging
To be able to convert an e-mail into an SMS message, the corresponding service must be registered with the provider. The following sections describe the procedure taking the example of T-Mobile as the provider.

3.1 Enable e-mail reception with a provider
Send an SMS message from your mobile phone with the text "OPEN" to the T-Mobile abbreviated dialing number 8000. This opens your T-Mobile number for e-mail reception.
Your e-mail address is then:
T-Mobile number (incl. prefix)@t-mobile-sms.de
017100000000@t-mobile-sms.de, for example.

Up to 160 characters are transferred.

3.2 Disable e-mail reception
If you no longer wish to receive e-mails, send an SMS message from your mobile phone with the text "CLOSE" to the T-Mobile abbreviated dialing number 8000.

This procedure might differ with other mobile network operators.
 
4. Other providers for SMS messaging
The list below is only a small selection of possible providers. Contact your provider for detailed information. Obtain information via the function:
"Enable mobile phone to receive e-mails from the Internet".

5. Download
The download includes a sample project for sending e-mails to a mobile telephone.
 Registration required SMS_Versand_PC.zip (2.4 MB)

Further Information
More information on the topic of "Teleservice via the Internet" is also available in Entry ID 19865167.

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit