×
Siemens Industry Online Support
Siemens AG
文档类型 常问问题 文档编号 2123168, 文档发布日期 2000年4月19日
(18)
评估

Resetting the S7-200 to the factory default settings (WIPEOUT)

  • 文档
  • 涉及产品

QUESTION: -

ANSWER:
"wipeout.exe" is a DOS application with which you can reset the target system (S7-200) to the factory default settings. This program is very useful if you have a target system with an unknown address or baud rate and cannot communicate with the target system using the STEP 7 Micro/Win. WIPEOUT deletes

  • The user program (OB1)
  • The data block (DB1) and
  • All configuration information (SDB).

The target system is set with address 2 to 9600 baud. WIPEOUT is not installed in conjunction with STEP 7-Micro/WIN 32. A copy of this application is on the Installation CD of STEP 7 Micro/WIN 32.
The program can be copied onto the hard disk and then called from there. To call the program, open the DOS window and enter the "WIPEOUT" command with the corresponding path. Then follow the prompts on the screen.

 wipeout.exe (45 KB)

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。