×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21298126, Entry date: 03/17/2009
(0)
Rate

How can you install WinCC flexible from the hard disk?

  • Entry
  • Associated product(s)

Below we provide version-related information on WinCC flexible for the case that you wish to install directly via the hard disk. 

  • WinCC flexible 2004
  • WinCC flexible 2005
  • WinCC flexible 2007
  • WinCC flexible 2008

Instructions for WinCC flexible 2004:
If WinCC flexible 2004 is to be installed directly from the hard disk, you must first create two new folders on the hard disk.
The first folder must be called "disk1" and the second "disk2".
The data of the first installation CD is to be copied into the "disk1" folder and the data of the second into the "disk2" folder.
You start the installation from the "disk1" folder via the Setup.exe file.

Instructions for WinCC flexible 2005:
If WinCC flexible 2005 is to be installed directly from the hard disk, you must first create two new folders on the hard disk.
The first folder must be called "CD_1" and the second "CD_2".
The data from the first installation CD is to be copied into the "CD_1" folder, and the data from the second into the "CD_2" folder.
Start the installation from the "CD_1" folder via the Setup.exe file.

Instructions for WinCC flexible 2007:
If WinCC flexible 2007 is to be installed directly from the hard disk, you must first create a folder, e.g. "WinCC_flexible_2007", on drive C:\.
Copy the complete contents of the installation DVD into this folder.
Start the installation from the "CD_1" folder via the Setup.exe file.

Instructions for WinCC flexible 2008:
If WinCC flexible 2008 is to be installed directly from the hard disk, you must first create a folder, e.g. "WinCC_flexible_2008", on drive C:\.
Copy the complete contents of the installation DVD into this folder.
Start the installation from the "CD_1" folder via the Setup.exe file.