×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 21331363, Entry date: 08/15/2019
(6)
Rate

Monitoring a protective door up to PL e / SIL 3 with a fail-safe S7-1500 controller

  • Entry
  • Associated product(s)
To prevent access to the danger range of a machine, a protective door is installed. The machine can only be started, if the protective door is closed. If the protective door is opened during operation or if an error is detected, the machine will be shut down safely.

Monitoring of the protective door position is designed according to EN ISO 13849‑1:2015 for requirements up to PL e and according to EN 62061:2005/A2:2015 for requirements up to SIL 3.

To ensure the required safety, the position of the protective door is monitored by two SIRIUS 3SE5 position switches. If one position switch fails, the second position switch still recognizes that the protective door is opened. The discrepancy monitoring in the controller detects a failure of one position switches and prevents that the system is switched on again until the error is eliminated.

In order to prevent failures of a common cause, position switches with different operating principles are used. In case of the position switch of position 1 the protective door position is detected via a separate actuator which is moved into the position switch when the protective door is being closed. The position switch of position 2 is provided with a swiveling lever which is actuated when the protective door is open.

In both position switches, a NC contact is evaluated each and assigned to the fail-safe digital input module. The controller detects cross-circuits between the two signals of the position switches.




Documentation and Project
  Documentation (1,0 MB)
 Registrierung notwendig  Example project for TIA Portal V15.1 (4,4 MB)
 Registrierung notwendig  Evaluation of the safety function as SET project (12,3 KB)



Last Changes
Update TIA Portal V15.1
Replacing components by SIMATIC S7-1500 with central modules


Additional Keywords
Safety door, safety-switch, safety-door, safety switch

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.