×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21383118, Entry date: 02/07/2017
(0)
Rate

Increasing the endurance of fuseless load feeders by using larger contactors

  • Entry
  • Associated product(s)
This article contains information on the dynamic behavior of various types of contactors.

QUESTION:

Can larger contactors than the types listed in the tables of the following publications be used for the purpose of increasing the electrical endurance of fuseless motor feeders with type of coordination 2? *Configuration manual "SIRIUS Configuration – Selection Data for Fuseless Load Feeders" * and *Configuration manual "Configuring SIRIUS Innovations" *



ANSWER:

Since the dynamic response of different types of contactors varies greatly, only the contactor tested in combination with the motor starter protector may be used. As a rule, the contactors required for type 2 have been designed to perform over and above the switching capacity (AC-3) defined for this type, thus already ensuring increased electrical endurance.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.