×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 21383151, Entry date: 11/29/2016
(4)
Rate

Fuseless Load Feeders for a 3-phase load with rated operational voltage of 230V AC?

  • Entry
  • Associated product(s)
This entry contains information about Fuseless Load Feeders with rated operational voltage of 230V AC

QUESTION:

Where can I find Fuseless Load Feeders for a 3-phase load with rated operational voltage of 230V AC?

 

 

ANSWER:

We recommend using standard 3RA2, 3RA1 load feeders as offered for a rated operational voltage of 400V AC. Simply use the current rating instead of the power (kW) rating for the selection of the suitable feeder combination.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.