×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21453120, Entry date: 04/06/2005
(0)
Rate

3UF5: SIMOCODE-DP 3UF5: Connection / Processing of an external fault signal

  • Entry
  • Associated product(s)
QUESTION:
SIMOCODE-DP 3UF5: Is the connection and processing of external speed monitor signals possible? If this monitor does not supply any more signals, an error message must be issued via bus system.

ANSWER:
The external signal must be connected to a free input of SIMOCODE. If only one message has to be transmitted via PROFIBUS the input-bit must be brought to a DP-output-bit.
If SIMOCODE has to switch off, the input-bit nust be brought to EXT.ERROR.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.