×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 21480479, Entry date: 05/30/2005
(0)
Rate

SIMATIC WinCC V6.0 SP3 Hotfix 2

  • Entry
  • Associated product(s)





DESCRIPTION:

The Hotfix 2 for SIMATIC WinCC V6.0 SP3 can now be downloaded by all customers. The Hotfix corrects problems that may occur during the archive configuration, alarm configuration and in VBS. The Hotfix may not be used with PCS7. 

All WinCC V6.0 SP3 packages delivered in the future will already come with the Hotfix 2. The revised product CD-ROM is labeled SIMATIC WinCC V6.0 SP3 incl. HF2. Hotfix 2 represents an officially released version, i.e. a conversion to the revised product version (SIMATIC WinCC V6.0 SP3 incl. HF2) is not required.  
 

Download of Hotfix 2

WinCC_V60_SP3_Hotfix2.exe ( 8158 KB )  






Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.