×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 21536617, Entry date: 03/28/2011
(0)
Rate

Which function modules (FM) can be used remotely in an ET 200M?

  • Entry
  • Associated product(s)

Configuration Notes
This entry provides information about which function modules can be configured in an ET 200M remote IO system and which can then be operated remotely.

Below is a list of the function modules that can be configured and used behind the PROFIBUS interface modules of the ET 200M.
In the compatibility list a difference is made between configuration via the metaknowledge integrated in STEP 7 and GSD configuration.

21536617_Compatibility_FM_with_PROFIBUS_InterfaceModules_en.pdf ( 83 KB )

In the entry below is a list of the function modules that can be configured and used behind the PROFINET interface modules of the ET 200M: 45313498.

Note
The entry below provides you with more information about function modules which use the functions "Read data record" and "Write data record": 15364459.
The entry below provides more information about using a positioning module FM 357-2: 21385102.

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.