×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 21656061, Entry date: 05/30/2005
(0)
Rate

3VF: Time discrimination between upstream fuses and downstream 3VF Circuit-Breakers?

  • Entry
  • Associated product(s)
QUESTION:
What is the time discrimination between upstream fuses and downstream 3VF circuit-breakers?

ANSWER:
Discrimination between upstream fuses and downstream 3VF circuit-breakers:--------------------------------------------------------------------------------------Overcurrents:Discrimination is provided if the tripping characteristics of both protection devices do not touch each other. The tripping characteristic of downstream circuit-breakers must be quicker than that of the upstream fuses.--------------------------------------------------------------------------------------Short-circuit currents:It must be taken into consideration that fuses are still heated up during the arc quenching process of the circuit-breaker. In practice it is sufficient if the tripping characteristic of the instantaneous release of downstream circuit-breakers is at least 70 ms quicker than that of the upstream fuses.--------------------------------------------------------------------------------------
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.