×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 21669390, Entry date: 06/27/2005
(0)
Rate

Easy Motion Control : Closed-Loop Controlled Positioning of an Axis with S7 300 CPU 314C-2 DP, MICROMASTER 440 and SIMATIC Easy Motion Control

  • Entry
  • Associated product(s)

Note
Effective October 1st, 2017 the MICROMASTER 4 standard drives are managed as a product to be phased out - see entry ID 109744726.
This means the MM4 standard drives should not be applied in new projects any more.
Drives from the SINAMICS G120 family can be used as alternative. Further information on this change you can find on the MICROMASTER Internet page www.siemens.com/micromaster.

Similar application examples for positioning :

Position Control with SIMATIC S7-1200 TO and SINAMICS V90 PN
Positioning a S120 (Startdrive) with SIMATIC S7-1500 (TO)
Positioning a G110M/G120 (Startdrive) with S7-1500 (TO) via PROFINET/PROFIBUS

-------------------------------------------------------------------------------------------------------------------------------------
Problem:  
The function mechanisms of closed-loop control positioning, which is frequently used, are illustrated technically taking a storage lift as an example, using a compact controller, SIMATIC Easy Motion Control software and a MICROMASTER.

Solution:  
Three automation solutions are described for this, containing details about the list of components, prices and function differences. The automation solution illustrated in the picture below has also been applied on the basis of a storage lift. To facilitate this, the S7 project contains a STEP 7 user program that positions a linear axis by means of closed-loop control with the aid of SIMATIC EASY MOTION CONTROL software. ProTool/Pro is used as a user interface. To aid your understanding of the system environment, an EXCEL worksheet enables you to read the distance traveled from the controller via an OPC link and displays this data diagrammatically. To demonstrate potential areas of application and restrictions under real conditions, the positioning accuracy has been measured under different load conditions, and the degree to which it can be transferred to more high-performance applications has been discussed.

 

Content of Downloads

 

Download
Documentation (German)
The documentation has been divided into 2 parts; the Application Description with information about the technological problem and the function mechanisms of the solutions, and the Parameterization Guide with information about the configuration of the MICROMASTER.
Application Description 21669390_GeregeltesPosEasyMC_DOKU_v10_d.pdf ( 2800 KB )
Parameterization Guide 21669390_GeregeltesPosEasyMC_Parametrierungen_DOKU_v10_d.pdf ( 1561 KB )
Documentation (English) 
The documentation has been divided into 2 parts; the Application Description with information about the technological problem and the function mechanisms of the solutions, and the Parameterization Guide with information about the configuration of the MICROMASTER.
Application Description 21669390_GeregeltesPosEasyMC_DOKU_v10_e.pdf ( 3767 KB )
Parameterization Guide 21669390_GeregeltesPosEasyMC_Parametrierungen_DOKU_v10_e.pdf ( 2737 KB )
S7-Code (archive of project)
STEP7 user program, visualization via ProTool/Pro and configuration data for MM440
 (The configuration data for MM440 included in the project can only be used with the software Drive-ES)
21669390_GeregeltesPosEasyMC_CODE_v10.zip ( 1043 KB )
Configuration data for MICROMASTER MM440
for the configuration tool Starter, if Drive-ES is not used)
21669390_GeregeltesPosEasyMC_MM440_Starter_CODE_v10.zip ( 40 KB )
EXCEL-worksheet (Deutsch)
 for measuring
21669390_GeregeltesPosEasyMC_MeasureData_TAB_v10_d.xls ( 373 KB )
EXCEL-worksheet (Englisch) 
 for measuring
21669390_GeregeltesPosEasyMC_MeasureData_TAB_v10_e.xls ( 379 KB )

 

History
 

Version

Modification

11/2003 first edition

 



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.