×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21739052, Entry date: 07/04/2005
(0)
Rate

How can you tell that WinCC has received data from AR_SEND (SFB37)?

  • Entry
  • Associated product(s)

Instructions:
If the data has been sent successfully to WinCC, the parameter "DONE" of the AR_SEND block is set to "1". In WinCC there is no way of checking whether the data has been stored successfully in the archive.

Note:
If the data has its own time stamp in AR_SEND, it is also stored chronologically in WinCC.  Detailed information on parameterizing the AR_SEND block is available in the WinCC Information System (WinCC Online Help) under the keyword "AR_SEND: Data Block Structures - Structures and Parameters". Note the examples given there.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.