×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 21767896, Entry date: 11/10/2005
(0)
Rate

How can the SINAMICS S120 drive system be commissioned with the configuration tools of the technology CPU?

  • Entry
  • Associated product(s)

Instructions:
In a complete answer to the question above, follow the instructions and directions in the document attached.

  • Operation of SINAMICS S120 (Firmware V2.2) with the Technology CPU (S7-Technology V2.0 SP1)
    Attachment 1: PDF-File ( 2194 KB )
     

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.