×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 217845, Entry date: 05/07/2008
(1)
Rate

How do you connect a PG 6xx and a PG 7xx?

  • Entry
  • Associated product(s)

Description:
You can connect the PG 6xx and PG 7xx with different modules. All the information you need for this is available in this FAQ:

How do you connect the PG 675/685 and the PG7xx programming devices to the PLCs S5 150A/K/U/S, S5 130WB and S5 110S?

Description:
There are no problems when setting up connections from the PG 675/685 and the PG 7xx programming devices to the PLCs S5 150A/K/U/S, S5 130WB and S5 110S?
Since the PLCs have an interface module AS 511 (25-pin), it is possible to connect the PGs. You must just pay attention to the following.

  • You only need plug-in connecting cable 6ES5 731-0xxx0 for PGs 675 and 685.
  • If you want to connect a PG 7xx, you need the adapter 6ES5 731-6AG00 in addition to the plug-in connecting cable 6ES5 731-0xxx0. There is no direct cable available for the PGs 7xx, but it can be made following the attached cable assignment diagram.

d_7xx511.pdf ( 6 KB )

What should you pay attention to when making a cable connection from PG 6xx to AS 511 - interface module (AG 130 / AG 150)?

To make the connection cable, you need a 25-pin Sub-D plug on the PG side and a 25-pin Sub-D socket on the side of the AS 511 interface module. The attached file "d_6xx511.pdf" shows the wiring.

d_6xx511.pdf ( 7 KB )  

What connection cable do you need between the PG 6xx and the programmable controllers AG 90 U to AG 155 U?

To make the connection cable, you need a 25-pin Sub-D plug on the PG side and a 15-pin Sub-D plug on the side of the PLC.

d_6xxagu.pdf ( 7 KB )  

How should the interfaces of a CP525 and a PG 6xx/7xx be connected with each other?

The cable layout plans below show you the relevant connections.

Connections between CP525 and a PG 6xx

CP525-PG6xx_d.pdf ( 3 KB )  

Connections between CP525 and a PG 7xx

CP525-PG7xx_d.pdf ( 4 KB )  

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit