×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 21848242, Entry date: 12/20/2012
(3)
Rate

How do you read consistent data from a DP standard slave/PROFINET IO device and write it consistently to a DP standard slave/PROFINET IO device?

  • Entry
  • Associated product(s)
Reading consistent data from a DP standard slave/PROFINET IO device and writing it consistently to a DP standard slave/PROFINET IO device.

SFC 14 "DPRD_DAT"
Using the system function SFC 14 "DPRD_DAT" (read consistent data of a DP standard slave) you read out the data of a DP standard slave/PROFINET IO device. If no errors occurred during the data transfer, the data read is entered into the target area set up by RECORD. The target area must have the same length as you configured with STEP 7 for the selected module. With a DP standard slave with modular structure and with multiple DP identifications, with an SFC 14 call you can only ever access the data of one module / DP identification under the configured start address.

SFC 15 "DPWR_DAT"
Using the system function SFC 15 "DPWR_DAT" (write consistent data to a DP standard slave) you transfer the data in RECORD consistently to the addressed DP standard slave/PROFINET IO device. The source area must have the same length as you configured with STEP 7 for the selected module.
With a DP standard slave with modular structure you can only access one module of the DP slave.

Maximum length and addressing of consistent user data areas on the PROFIBUS DP
In the manuals listed below you will find more information about the maximum length and addressing of consistent user data areas on the PROFIBUS DP.
 

Manual Chapter/Section Entry ID
SIMATIC S7-300 CPU 31xC and CPU 31x: Configure Addressing

13008499

SIMATIC Distributed IO ET 200S Interface Module IM151-7 CPU Addressing

56046285

SIMATIC Distributed IO ET 200S Interface Module IM151-8 PN/DP CPU Addressing

47409312

SIMATIC ET 200pro Interface Module IM 154-8 PN/DP CPU Addressing 44251850
SIMATIC Basic Module BM 147/CPU Addressing

1142364

SIMATIC S7-400 Automation System S7-400 CPU Specifications Consistent Data

53385241

Table 01

Maximum length and addressing of consistent user data areas on the PROFIBUS IO
In the manuals listed below you will find more information about the maximum length and addressing of consistent user data areas on the PROFIBUS.
 

Manual Chapter/Section Entry ID
SIMATIC S7-300 CPU 31xC and CPU 31x: Configure Addressing

13008499

SIMATIC Distributed IO ET 200S Interface Module IM151-8 PN/DP CPU Addressing

47409312

SIMATIC ET 200pro Interface Module IM 154-8 PN/DP CPU Addressing

44251850

SIMATIC S7-400 Automation System S7-400 CPU Specifications Consistent Data 53385241
Table 02

For communication processors (CPs) the size of the consistent area for a submodule is defined as follows.
 

CP Article number Upper limit
CP 443-1 6GK7443-1EX20-0XE0 240 bytes
CP 443-1 6GK7443-1EX30-0XE0 240 bytes
CP 443-1 Advanced 6GK7443-1EX40-0XE0 128 bytes
CP 443-1 Advanced 6GK7443-1EX41-0XE0 240 bytes
CP 443-1 Advanced 6GK7443-1GX20-0XE0 240 bytes
CP 443-1 Advanced 6GK7443-1GX30-0XE0 240 bytes
CP 343-1 6GK7343-1EX21-0XE0 128 bytes
CP 343-1 6GK7343-1EX30-0XE0 240 bytes
CP 343-1 Advanced 6GK7343-1GX21-0XE0 128 bytes
CP 343-1 Advanced 6GK7343-1GX30-0XE0 240 bytes
CP 343-1 Advanced 6GK7343-1GX31-0XE0 240 bytes
Table 03

Notes
The PROFIBUS DP standard defines upper limits for the transfer of consistent user data. Current DP standard slaves keep to these upper limits. Older CPUs (<1999) have CPU-specific restrictions for the transfer of consistent user data.
The maximum length of data that these CPUs can read consistently from a DP standard slave or write consistently to a DP standard slave is given in the technical data under "DP master – user data per DP slave". With this value, more recent CPUs exceed the length of the data that a DP standard slave provides or receives.

Important
Distributed reading and writing of consistent data (<4 bytes) is also possible without system functions SFC 14 and SFC 15. Which modules you can use for this is described in Entry ID 8751062.

The table below shows the access to consistent data outside the process image.
 

Length of data area Read/write access Data consistency
1 byte Load / Transfer Consistency over unit
2 bytes Word Load / Word Transfer Consistency over total length
3 bytes SFC 14 / SFC 15 Consistency over total length
4 bytes Double-word Load / Double-word Transfer Consistency over total length
5 bytes or more SFC 14 / SFC 15 Consistency over total length
Table 04

Example
In the example below an S7-400 CPU is used as DP master and a CP342-5 as DP slave.

The consistency area below is defined for the inputs and outputs of the DP slave:

  • For the outputs, 50 bytes are transferred consistently over the total length. These 50 bytes are available consistently in the process image partition 3 (PIP 3) of the S7-400 CPU and can therefore be read using load/transfer commands.
  • For the inputs, 20 bytes are transferred consistently over the total length. These 20 bytes are not stored in the process image or in process image partition and can only be written with the system function SFC 14/15.


Fig. 01

The operating system of the CPU transfers the data consistently during process image updating. You can access this data in the process image using the load and transfer commands.
Alternatively, with S7-400 CPUs you can use system function SFC 26 "UPDAT_PI" or SFC 27 "UPDAT_PO" at any point in the program to update the process images. However, in this case the relevant PIP may not be updated by the system. If you do not or cannot place the data in a process image, then you should use the system functions SFC 14 and SFC 15 for data communications.

More information on this is available in the following entries:

  • "Consistent data in S7-400, summary of mechanisms" - Entry ID: 11646774
  • "Use of Process Image Partitions in Organization Blocks" - Entry ID:18325216

 

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.