×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 21897529, Entry date: 05/22/2006
(0)
Rate

Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC?

  • Entry
  • Associated product(s)

Description:
In WinCC flexible 2004 / 2005 SP1 you have configured an OP73 / OP73micro / TP177A / TP177micro or OP77A. In the Engineering software the buttons and menu entries "Start Runtime" that are used for starting the Runtime simulation for other operator panels on the PC are grayed out and cannot be executed.

Explanation:
The Runtime simulation of an OP73 / OP73micro / TP177A / TP177micro or OP77A is not provided for in WinCC flexible 2004 nor in WinCC flexible 2005 SP1, so the corresponding selection options are grayed out and cannot be executed.

Note:
As of WinCC flexible 2007 it is now also possible to use the Runtime simulation of OP73 / OP73micro / TP177A / TP177micro or OP77A.

Remedy:
In order to be able to simulate the project nevertheless on the PC you can convert the operator panel into a comparable HMI device.

Procedure:
Open the project via "Project > Open" and then select "Project > Change Device Type...". Now select the relevant device type and confirm with "OK".
  

Operator panels without Runtime simulator

 

HMI device with Runtime simulator

OP73
OP73micro
OP77A
OP77B
TP177micro
TP177A
TP170A or TP177B

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.