Entry type: FAQ, Entry ID: 21915433, Entry date: 08/25/2005
(0)
Rate

Which settings are required to access an S7 CPU with WinCC and SIMATIC NET via a CP5611, CP5613 or CP1613?

  • Entry
  • Associated product(s)

Configuration Notes:
The steps below describe the procedure for a CP5613. The procedure applies accordingly to the other cards.
 

No. Procedure
1 Install SIMATIC NET.
2 Install the CP5613 in a free PCI slot.
3 Start the PC.
4 After the PC has started up, SIMATIC NET automatically starts the Commissioning Wizard and recognizes the CP5613.
5 Assign the required addresses and parameters to the card and enable the option "Use module only for PG mode".


Fig. 01
 
 
6 Create a new project using the Configuration Wizard.
7 Follow the configuration wizard through to the end and load the parameters into the CP (menu item: "Load PLC > Load in module").
8 Set the access points for the CP in the Configuration Console.


Fig. 02
 
 
9 Select the relevant card and open the Properties ("Right-click > Properties").
10 Assign the appropriate interface parameters to the card.


Fig. 03
 
 

Note:
If some of the settings are to be entered later, you can call these dialogs again via "Start > SIMATIC > SIMATIC NET > Settings > Commissioning Wizard".

11 In the WinCC Explorer under "Tag Management" you configure the channel for your CPU and enter the associated device names in the system parameters.


Fig. 04
 
 
12 Configure tags and pictures.
 

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster