×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 21971330, Entry date: 08/26/2005
(0)
Rate

SIMATIC WinBDE V7.2 SP2 available now (Delivery Release)

  • Entry
  • Associated product(s)

 

Effective immediately, SIMATIC WinBDE V7.2 SP2 is released for delivery. The order numbers remain unchanged.

 



New in Version 7.2 SP2

WinBDE V7.2 SP2 is also released for use as an option with 

  •     WinCC flexible 2005
  •     WinCC V6.0 SP3

In addition to the previously supported operating systems, the operation under Windows XP Professional SP2 has been released as well

The function scope remains unchanged compared to WinBDE V7.2 SP1.

Upgrade - free Update from V7.2 to V7.2 SP2

Customers already employing V7.2 can order the Service Pack 2 for V7.2 of WinBDE free of charge after presenting the original delivery bill or software product card of the respective software package.

Request Form ( 68 KB )

Because of the delivery form, no Internet download is possible. 

Note:
For the installation, please observe the information contained in the document "doc/WinBDE_V7.2_SP2_english.pdf" (chapter 2) on the supplied CD-ROM.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.