Entry type: FAQ, Entry ID: 21975526, Entry date: 07/08/2013
(0)
Rate

Why do you get the message "Under Construction" in WinCC flexible when attempting to connect to the MiniWeb with the HTML viewer?

  • Entry
  • Associated product(s)

Description
The "Under Construction" message can be displayed among other things if "Internet Information Service (IIS)" is installed.

If, for example, you are using the "WinCC Web Navigator Server", then when the "Sm@rt Service (HTML pages)" function is started and the "IIS" is active, the "Under Construction" message is displayed.
The reason for this is that both services, the IIS service and the "Sm@rt Service (HTML pages)", access Port 80.

Sample case for possible error messages:
 

No.  
1 "IIS" is enabled
  • "IIS" is enabled and an attempt is made to start the "Sm@rt Service (HTML pages)" function.
    The "Under Construction" message appears.


Bild 01
2 "Sm@rt Service (HTML pages)" is enabled
  • "Sm@rt Service" is enabled and an attempt is made to start the "IIS" function.
    The "Unexpected error 0x8ffe2740" message appears.


Bild 02
  • In Windows 7 this message is displayed: "Error executing this procedure". Details: The process cannot access the file, because it is being used by another process".

Remedy
There are different ways of clearing this behavior.

 

No. Check whether the "IIS" is enabled/disabled
1

Check whether the service is executed when IIS is installed.

Windows XP

  • "Start > Programs > Administration > Internet Information Services" 
  • You can insert the "Administration" view with
    "Start > Settings > Taskbar and Start menu". 
    Go to the tab "Start menu > "Change" button" and switch to
    "Advanced Start menu options". There you select "Display administration".


Bild 03

"IIS" enabled


Bild 04

"IIS" disabled


Bild 05

Note
To deactivate or activate the IIS you mark the "Default Web Site".
You can now start or terminate the IIS with a right-click.
This option does not work if you are using an embedded operating system. To disable the service you must change the setting under "Start > Control Panel > Administrative Tools > Services > Internet Information Service".

Windows 7

  • "Start > Control Panel > Administration > Internet Information Services (IIS) Manager".
  • To view the status of the Internet Information Service you start the Internet Information Service with "Internet Information Services (IIS) Manager".
  • Double-click the connection.
  • Click "Sites".
  • Right-click "Default Web Site > Manage web site "; here you can "Start" or "Terminate" the service.

 

No. Change the port for the IIS
1

You can change the port address for the IIS as follows.

Windows XP

  • "Start > Programs > Administration > Internet Information Services" 
  • You insert the "Administration" view with
    "Start > Settings > Taskbar and Start menu". 
    Go to the tab "Start menu > "Change" button" and switch to
    "Advanced Start menu options". There you select "Display administration".
  • Open the "Website" folder and have the properties of the "Default Web Site" displayed.
  • You can change the address in the subdirectory "Website" > "TCP port".


Bild 06

Windows 7

  • "Start > Control Panel > Administration > Internet Information Services (IIS) Manager".
  • Start the Internet Information Server (IIS) with "Internet Information Services (IIS) Manager".
  • Double-click the connection.
  • Click "Sites".
  • Right-click "Default Web Site > Connections...".
  • In the window that opens you click the connection.
  • Click "Edit...".

 

No. Deinstall the IIS
1

Check whether the Windows component "Internet Information Services" (IIS) is installed.

 Windows XP

  • "Start > Settings > Control Panel > Software"
  • Click the "Add/Remove Windows Components" button.
  • Is Internet Information Services (IIS) selected in the dialog window that opens?

If you do not need Internet Information Services (IIS), you can remove the check mark next to "Internet Information Services (IIS)".
Then click the "Next >" button and the program is deinstalled.


Bild 07

If you need Internet Information Services (IIS) again, you can set a check mark next to "Internet Information Services (IIS)".
Then click the "Next >" button and the program is installed.

Note
You might need the Microsoft Windows XP CD to install the IIS.

Windows 7

  • Click "Enable/Disable Windows Functions".
  • Here you use the check box to install or deinstall Internet Information Services.  

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster