×
Siemens Industry Online Support
Siemens AG
Type de contribution : FAQ ID de la contribution : 22036987, Date de la contribution : 22/12/2015
(2)
Évaluer

What is to do if I want to project, set up and place on the market a legal for trade scale?

  • Contribution
  • Concerne le/les produits(s)
QUESTION: What is to do if I want to project, set up and place on the market a legal for trade scale? ...

QUESTION:  

What is to do if I want to project, set up and place on the market a legal for trade scale?

ANSWER:

In the attached checklist you will find all important items that you have to care for.

To facilitate you the calibration procedure, you can order a verification / calibration set with the order no. 7MH4 900-2AY10, this contains the material for the commissioning of up to 5 legal for trade scales, consisting : 1x Labelling film for the labelling sign, 1x protection film, instructions for the verification/calibration, certificates and pattern approvals, editable labelling sign models, SIWAREX FTA manual and Siwatool V4 on CD.

If you have more questions you can contact the SIWAREX Hotline
+49 721 595-2811 or hotline.siwarex@siemens.com

Download Checklist for calibratable scales

  Checkliste_AWI_NAWI_en.pdf (163,3 KB)

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.