×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 22054730, Entry date: 09/20/2005
(0)
Rate

Release for general availability for Drive ES Basic V5.3 SP3

  • Entry
  • Associated product(s)

This update info releases the Drive ES Basic V5.3 SP3 product for general availability.
The reasons for the revision and ongoing development is the fact that STEP7 V5.3 SP3
has been launched into the market and the functionality of the integrated
commissioning tool has been further expanded.

 Release for general availability on 08.09.2005.

 Order Nos. [MLFBs]:

Order No.

Product

 

 

 Availability

6SW1700-5JA00-3AA0

Drive ES Basic V5.3 SP3, single license

 

 

 Available immediately

6SW1700-0JA00-0AB2

Software update service for
Drive ES Basic, single license

 

 

Available immediately

6SW1700-5JA00-3AA1

Copy license (60 installations)
Drive ES Basic V5.3 SP3

 

 

Available immediately

6SW1700-0JA00-1AB2

Software update service for Drive ES Basic, copy license

 

 

Available immediately

6SW1700-5JA00-3AA4

Upgrade Drive ES Basic V5.x to V5.3 SP3 for a single license

 

 

Available immediately

The reasons for the revision and ongoing development is the fact that STEP7 V5.3 SP3
has been launched into the market and the functionality of the integrated
commissioning tool has been further expanded.
The following individual innovative functionality has been incorporated:

  • Fully compatible to STEP7 V5.3 SP3
  • Starter Version V3.2 SP1, the commissioning tool for SINAMICS and MICROMASTER 4th generation have been integrated.
  • SimoCom A Version V 04.03.00, the tool for POSMO A, has been integrated.
  • SimoCom U Version V 08.03.07, the tool for SIMODRIVE 611U and POSMO CA/CD/SI, has been integrated.
  • New DriveMonitor Version V5.3 SP2 HF3, the tool for MASTERDRIVES and SIMOREG, has been integrated.  

New features of the integrated DriveMonitor V5.3 SP2 HF3:

·2 buttons have been included in the symbol bar; these can be used to directly run frequently used scripts from the symbol bar.

·Otherwise, no functional changes have been made to DriveMonitor V5.3 SP2. 

Additional information on the integrated DriveMonitor Version V5.3 SP2 is available under ProdIS-ID: 20145460

New functionality for the integrated Starter V3.2 SP1:

From the new Starter V3.2 SP1 onwards ( V3.2.1.x ), the following drive systems are now supported: 

·All drive units belonging to MICROMASTER 4th generation

·SINAMICS G110 V1.0x and V1.1x 

·SINAMICS S120 V2.1.x to V2.3.x

·SINAMICS G150 V2.1.x to V2.3.x

·SINAMICS S150 V2.1.x to V2.3.x

·SINAMICS G130 V2.1.x to V2.3.x

·SIMATIC ET200S FC with firmware V1.0x

Additional information on the integrated Starter Version V3.2 SP1 is available under ProdIS-ID: 21914503

The integrated commissioning tools can be individually downloaded from the Internet and in this way can be used as free-of-charge upgrade of an existing Drive ES Basic V5.3 SPx software installation.

How do I get the new version?

Order it from new!
All orders are supplied with this release for general availability.  The price remains the same.

For users that already have a version of Drive ES Basic V5.X!
Can be ordered using the upgrade version. This is available at a significantly lower price than the full version. 
It is not possible to download the complete Drive ES Basic CD V5.3 SP3 for reasons relating to the memory space required.
It can only be ordered using the upgrade version. This is available at a significantly lower price than the full version.

For those in possession of an update service contract 6SW1700-0JA00-0AB2 or 6SW1700-0JA00-1AB2!
Those in possession of an update service contract will automatically receive the new version.

Compatibility:
Windows 2000, XP Professional incl. SP2
STEP7 V5.2 SP1 and STEP7 V5.3 and V5.3 SPx
Detailed information regarding the compatibility is provided in ID 18495518

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.