Entry type: FAQ, Entry ID: 22057057, Entry date: 05/03/2013
(1)
Rate

Why can ProTool no longer be started from STEP 7 after WinCC flexible has been installed?

  • Entry
  • Associated product(s)

Description
If you install WinCC flexible on a computer on which ProTool is already installed, under certain circumstances ProTool can no longer be started from STEP 7. You can use the following remedies for this:

Note
Pay attention to the compatibility of the products STEP 7, WinCC flexible and ProTool in Entry ID: 64847781. For example, the versions STEP 7 V5.5, WinCC flexible 2008 SP3 and ProTool V6.0 are not compatible.

WinCC flexible 2008
 

No. Action
1. Call ProTool once via the Windows Start menu after installing WinCC flexible.
2. Open the ProTool project from STEP 7.

WinCC flexible 2008 SP2

Remedy 1
 

No. Action
1. Open the STEP 7 Manager.
2. Select the menu command "Help > About...".
3. Click on the "Update menus..." button.

Remedy 2
 

No. Action
1. Uninstall ProTool as described in Entry ID:18697689.
2. Install ProTool.
3. Start ProTool and create a new project.
4. Close ProTool (no need to save the project).

Remedy 3
 

No. Action
1. Uninstall ProTool as described in Entry ID:18697689.
2. Install ProTool.
3. Start ProTool and create a new project.
4. Close ProTool (no need to save the project).
5. Open the STEP 7 Manager.
6. Select the menu command "Help > About...".
7. Click on the "Update menus..." button.

 

Workaround
Open the ProTool project by double-clicking on the ProTool operator panel in NetPro.

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster