×
Siemens Industry Online Support
Siemens AG
Entry type: Download, Entry ID: 22072983, Entry date: 03/29/2012
(0)
Rate

Operating System Updates for ET200S 1PosU

  • Entry
  • Associated product(s)

DESCRIPTION:

When updating the operating system, always update to the latest version available for the product and its respective order number. The previous versions of the operating system are only intended as backup to allow a downgrade to the original version - there are however no known cases where this has been necessary.

 

Note:
- Firmware 
V2.0.0 (delivery state with product release version 8) and higher can only be
   loaded onto modules with a product release version of 8 or higher
- Firmware V1.x.x can only be loaded onto modules with product release versions from     1 up to and including 7
- Product release versions 5, 6 and 7 were skipped for internal reasons
 

Online Firmware Update by means of STEP 7 HW-Config:

  1. Download the desired firmware file
  2. Unpack the file by double-clicking on the file name
  3. In HW-Config, select the module from the ET200S station 
  4. Program the firmware by selecting "Target System/Update Firmware" in the program menu
  5. In the dialog box, select the folder with the firmware file and start the firmware download

After completion of the download, the new firmware can be started automatically or via a power OFF/ON.

Note:
The firmware update can be performed with the following interface modules:

  • IM151-1/Standard from 6ES7151-1AA04-0AB0
  • IM151-1/High Feature from 6ES7151-1BA01-0AB0


Overview of order numbers and latest versions of the 1PosU:

Order Number

FW
Version

Update

6ES7138-4DL00-0AB0

   
 

V1.0.1

Recommended as Update:

Update V1.0.1 Description

  1384DL00_V101.EXE ( 91 KB )

 

V1.0.0

Backup only:

  1384DL00_V100.EXE ( 91 KB )



 

 

Update V1.0.1 (6ES7 138-4DL00-0AB0)



Correction of the startup behavior:
When powering on the module while a load voltage is present, the error
ERR_2L+ (Load Voltage 2L+) is now no longer reported for up to 8 seconds.


Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.