×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 22078757, Entry date: 03/21/2014
(7)
Rate

MICROMASTER 4 & SINAMICS G120: Function block (FC14) to control an MM4 via PROFIBUS DP

  • Entry
  • Associated product(s)

Note
Effective October 1st, 2017 the MICROMASTER 4 standard drives are managed as a product to be phased out - see item ID 109744726.
This means the MM4 standard drives should not be applied in new projects any more.
Drives from the SINAMICS G120 family can be used as alternative. Further information on this change you can find on the MICROMASTER Internet page www.siemens.com/micromaster.

A similar SINAMICS G120 Application example for "Function block to control an MM4 via PROFIBUS DP" you can find at item ID 109475044.
-------------------------------------------------------------------------------------------------------------------------------------


Task
A MICROMASTER 4 or a SINAMICS G is quickly and simply to be coupled to a SIMATIC S7-300/400 control via Profibus-DP. The user shall be provided with a simple control and setpoint interface.

Validity
The example applies to an implementation with STEP 7 V5.x for all PROFIBUS-capable...

  • MICROMASTER 4
  • SINAMICS G120 / G120C / G120D

If you work with a SIMATIC S7-1200 or S7-1500 in the TIA Portal, we recommend to use the FB "SINA_SPEED" (FB285) from the library "DriveLib_S71200/1500...".
The function block and its description is installed together with Startdrive (Download under entry ID: 68034568) and is available as a global library in TIA Portal.
Alternatively, you can download the library (without Startdrive)  at entry ID 109475044.

Solution
The implementation is done with with function block FC14. The signals used are comparable with the control and setpoint interface via terminal strip.

Downloads

Content of Downloads

Download

Documentation 22078757_Function_block_to_control_MM4_via_PROFIBUS_DP_DOCU_v3_2_en.pdf ( 259 KB )
Project example for STEP 7 V5.x
(FC14_PROFIBUS_DP_en.zip)
FC14_PROFIBUS_DP_en.zip ( 479 KB )
Project example for STEP 7 V5.x
(FC14_DP_Ref_Freq_en.zip)
This project example uses a extended FC14 with a input for the reference frequency. See chapter 4 of the documentation for details.
FC14_DP_Ref_Freq_en.zip ( 480 KB )

Last Changes
Link to an implementation with S7-1200/1500 in TIA Portal, editorial revision


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.