×
Siemens Industry Online Support
Siemens AG
文档类型 应用实例与扩展工具 文档编号 22078991, 文档发布日期 2005年9月17日
(1)
评估

MICROMASTER 440: manually determining the magnetizing current and re-calculating the motor equivalent circuit diagram

  • 文档
  • 涉及产品

Exclusion:

This application only applies to MICROMASTER 4 with Firmware < V4.0

 

Description:

In order to successfully commission a drive system it is important that the rated motor data are correctly downloaded into the drive inverter and a motor identification routine carried-out. The procedure is described in Chapter 3.5 “Commissioning” of the Instruction Manual.

After the “Commissioning” phase has been successfully completed, for most applications the drive can be accelerated up to rated speed. Depending on the motor being used and the mechanical layout it may however be necessary to further optimize the individual controllers.

Especially for SLVC (sensorless closed-loop vector control), the feedback signals for the internal controllers depend on calculated quantities – such as flux actual value and speed actual value – from the motor model.

The value of the magnetizing current has a special influence on the control parameters. This cannot be measured at standstill. This is the reason that it is estimated using the automatic parameterization routine as typical value for a standard SIEMENS motor. Due to the difference between the “real” magnetizing current and the estimated magnetizing current, it is also not possible to precisely determine the values of the magnetizing reactance and rotor resistance.  This can result in difficulties when optimizing the drive - especially for third-party motors,(also refer to ID: 15293059).

The procedure to manually determine the magnetizing current, re-calculate the motor equivalent circuit diagram when the drive is operated with closed-loop vector control are described in the following.

Downloads

Content of Downloads

Download

Documentation (German) tipps_tricks_004_Ausmessen_des_Magnetisierungsstroms_update_de.pdf ( 102 KB )
Documentation (English) tipps_tricks_004_Measuring_magnetizing_current_update_en.pdf ( 108 KB )

 

History

Version

Modification

05/2003 first edition

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。