×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 22131351, Entry date: 10/15/2005
(0)
Rate

S7 Distributed Safety V5.4 Released for Delivery

  • Entry
  • Associated product(s)

S7-Distributed Safety V5.4 has been released for delivery. The software is multilingual (German, English, French) and is available on CD ROM as single license (Floating License) or upgrade, incl. the electronic user manuals. You will find the major additions and corrections in the attached list.


General

This software enables the creation of failsafe programs for controllers supported by S7 Distributed Safety. With S7 Distributed Safety and the supported controllers and signal modules you can build a failsafe programmable controller not only for classical failsafe automation tasks on machines and presses, but also for process control applications.

New features and functions:

·        Support of PROFINET IO

·        Support of failsafe IO standard devices

·        Support of individual channel passivation

the following modules presently support this function:

o      6ES7326-2BF01-0AB0

o      6ES7326-2BF40-0AB0

o      6ES7326-1RF00-0AB0

o      6ES7336-1HE00-0AB0

o      6ES7138-4FA02-0AB0

o      6ES7138-4FB02-0AB0

o      6ES7138-4CF02-0AB0

o      6ES7138-4CF41-0AB0

o      6ES7148-3FA00-0XB0

o      6ES7148-4FA00-0AB0

o      6ES7148-4FC00-0AB0

·        Failsafe I slave to slave communication

·        Support of failsafe communication via S7 connections for
CPU 315F-2 PN/DP and CPU 317F-2 PN/DP on the PN interface

·        Improved user desktop of S7 Distributed Safety

o      Generation of the complete failsafe program via the function "check block consistency"

o      Password allocation/interrogation for the failsafe program in HW Config

o      Enhanced comparison of failsafe programs in the dialog  "compare failsafe programs"

o      Additional compiler checks (direct access of std. program section to F resources, delta download)

Compatibility:

S7 Distributed Safety V5.4 is fully upwards compatible with S7 Distributed Safety V5.3. 


System prerequisites

STEP 7 V5.3 SP3
 

Ordering data:

Designation

Order No.

SIMATIC S7, Distributed Safety V5.4
FLOATING LICENSE FOR 1 USER

6ES7833-1FC02-0YA5

SIMATIC S7, Distributed Safety V5.4 UPGRADE
(V5.X  to V5.4) FLOATING LICENSE FOR 1 USER

6ES7833-1FC02-0YE5

SIMATIC S7, Distributed SafetySOFTWARE UPDATE SERVICE FOR 1 YEAR W. AUTOM. EXTENSION; REQUIRES LATEST  SW VERSION

6ES7833-1FC00-0YX2

 

Documentation:

The documentation for S7 Distributed Safety V5.4 is contained on the product CD ROM in the form of a pdf file. It can also be downloaded from the Internet under the entry ID 22099875.


For more information:


www.siemens.de/f-cpu


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.