×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22144502, Entry date: 04/12/2018
(41)
Rate

How do you configure your PC as NTP server?

  • Entry
  • Associated product(s)
The Network Time Protocol (NTP) is a standard for synchronizing computer system clocks over package-based communication networks.

Although this is usually done via UDP, it can also be transported by other Layer 4 protocols such as TCP, for example. It was specially developed to enable reliable time relaying via networks with variable package runtimes.

The Simple Network Time Protocol (SNTP) is a simplified version of NTP. It is described in RFC 2030. The Network Time Protocol (NTP) is described in RFC 958.

Instructions for the following Windows operating systems:

  •  Windows 2000

  •  Windows XP

  •  Windows Server 2003

  • Windows Server 2008 (32 Bit) 

Follow the instructions to configure your local PC as NTP server. In this way you can synchronize other devices with the local PC.

  1. Open the registry editor via "Start > Run... > regedit".
  2. Search for the code
    "HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\W32Time\Parameters".
  3. Set the "LocalNTP" value to 1.
     

    Fig. 01

    Note

    • If the "LocalNTP" value does not exist in your system, create a new DWORD value.

    • The value 0 means disabled, 1 means enabled

  4. Restart the computer to make the changes effective.


Instructions for the following Windows operating systems:


  • Windows 7 (32-bit and 64-bit)
  • Windows 10 (32-bit and 64-bit)
  • Windows Server 2008 R2 (64-bit)
  • Windows Server 2012 R2 (64-bit)
  • Windows Server 2016 (64-bit)

Follow the instructions to configure your local PC as NTP server. In this way you can synchronize other devices with the local PC.
 


  1. Stop the "Windows Time" service via Start > Control Panel > System and Security > Administrative Tools > Services.
       

    Fig. 02
       
  2. Open the registry editor via "Start > Run... > regedit".
     
  3. Search for the code "HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\services\W32Time\TimeProviders\NtpServer".
     
  4. Set the "Enable" value to 1.
     

    Fig. 03
     
  5.  Search for the code
    "HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\services\W32Time\Config".
     
  6. Set the "AnnounceFlags" value to 5.
      

    Fig. 04
        
  7. Start the "Windows Time" again and set the start type to "Automatic".
      
Note
  • When using the Windows server 2012 R2 (64-bit), after Step 7 you have to set the start type to "Automatic (Delayed Start)" for the service to start automatically.
  • If, when using Windows 7 or the Windows Server 2008 R2, the "Windows Time" service always stops, follow these instructions:
    https://support.microsoft.com/en-us/help/2385818

Follow the instructions below for configuring the "Windows Time" service when using an internal hardware clock and an external time source.

https://support.microsoft.com/en-us/help/816042

If the firewall is enabled, it must be configured to permit external access to Port 123. This is necessary because the time server service expects external request messages.

Warning
Changes in the Registry might lead to unexpected problems requiring you to reinstall your system. We cannot guarantee that problems arising from changes in the Registry can be solved. Changes in the Registry are made entirely at the user's own risk.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.