×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22149156, Entry date: 10/28/2005
(1)
Rate

How do you realize a sensor range of 4mA to 20mA with an analog module EM231 or EM235?

  • Entry
  • Associated product(s)

Instructions:
Use the DIP switches to configure a sensor range of 0mA to 20mA. Wire the sensor as shown in Fig. A-12 (Channel D) in Appendix A of the SIMATIC S7-200 Programmable Controller System Manual (Entry ID 1109582). Connect L+ of the power supply to the sensor's plus connection. Connect the sensor's minus connection to RD and D+. Connect all of the ground connections M together and connect them to D-.

Note:
When using a 4mA to 20mA sensor, you must convert the measured value accordingly. A sample program with explanations is available as Tip 38a in "Tips&Tricks S7-200" in Entry ID 1232912.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.