×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 22155058, Entry date: 10/13/2005
(0)
Rate

Update for the Device Library of SIMATIC PDM V6.0 + SP1 (as per 09/05)

  • Entry
  • Associated product(s)

DESCRIPTION:

The attached update is only of importance for SIMATIC PDM V6.0 + SP1 and higher. It is used to integrate the device descriptions of the new 8-channel HART analog modules SM 331 (AI 8 x 0/4...20 mA HART), order no. 6ES7 331-7TF00-0AB0, and SM 332 (AO 8 x 0/4...20 mA HART), order no. 6ES7 332-8TF00-0AB0, from the range of ET 200M distributed I/Os.

You can use the device descriptions of the updates to supplement the device library of SIMATIC PDM V6.0 + SP1 free of charge. Your existing licenses for SIMATIC PDM V6.0 remain valid. The device descriptions of the update will be included in SIMATIC PDM V6.0 when the device library is updated in due course.

Notes on the update of the device descriptions in conjunction with the update of the device library

The device library CD ROM of SIMATIC PDM is always updated together with the release of a new version or a ServicePack, or when required. It is published in a separate SIMATIC update or download entry. In the meantime new device descriptions can be released for SIMATIC PDM as update and integrated in the device library when it is updated later. As long as this integration has not taken place, these updates must be installed again after each new SIMATIC PDM installation.

Scope of supply:


The attached update (see download link below) for SIMATIC PDM V6.0 + SP1 is free of charge and includes the following additional device descriptions:
 

Company

Device Type

Version

Type

Communication

Remark

Siemens

SIMATIC ET 200M
8-channel HART module
AI 8 x 0/4...20 mA HART

1

SM

HART

newly included

Siemens

SIMATIC ET 200M
8-channel HART module
AO 8 x 0/4...20 mA HART

1

SM

HART

newly included

Installation:
Existing project data will be retained during the update procedure. Please read the installation instructions in the readme file of the product CD ROM of SIMATIC PDM V6.0 + SP1.

Procedure:

Unpack the zipped download file to a directory of your choice (e.g. C:\Temp).

Extract the two ZIP files created in the predetermined directory into two separate folders (e.g. "C:\Temp\PDMV60SP1HF1" for the Hotfix and "C:\Temp\ET200M_8kanal_HART" for the device descriptions)

Start the file "Setup.exe" in the Hotfix folder (e.g. C:\Temp\PDMV60SP1HF1) and follow the installation dialogs.

Use "Start -> SIMATIC -> SIMATIC PDM" to start the function "Administrate device library"

Open the folder with the device descriptions (e.g. C:\Temp\ET200M_8kanal_HART) and select "ET 200M"

Confirm any upcoming overwrite warning with "Yes"

Start the device import

General:
As long as the device descriptions are not integrated in SIMATIC PDM, the update procedure must be repeated after each new installation.

If you are using non-Siemens devices please read the notes concerning warranty and liability in chapter 4 of the "Readme file" of SIMATIC PDM (supplement to the "General Conditions for the Sale of Software for Automation and Drives").

More information on the individual devices is available from the relevant manufacturer.

Miscellaneous:
More device descriptions and information on field devices and components that can be processed with SIMATIC PDM are available from the Internet sites of the relevant manufacturer.
If you cannot find the field devices or components you wish to use in the SIMATIC PDM device library, please contact us. We will be glad to help you.

Contact address:

Siemens AG, Technical Support

Region

Europe

Asia/Pacific

America

Tel.

+49 180 50 50 222

+86 1064 719 990

+1 423 262 2522

Fax.

+49 180 50 50 223

+86 1064 747 474

+1 423 262 2289

E-mail

adsupport@siemens.com

adsupport.asia@siemens.com

simatic.hotline@sea.siemens.com

 

Update for 8-channel ET 200M HART analog modules

Update_ET200M_8kanalHart_PDM6.0SP1.zip ( 9762 KB )


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.