×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22158108, Entry date: 11/02/2005
(0)
Rate

How do you load a firmware update with the serial interface module ET 200S 1SI?

  • Entry
  • Associated product(s)

Instructions:
How to load a firmware update into the serial interface module ET 200S 1SI is described in detail in section 2.9.2 "Loading firmware updates" in the manual of the module concerned (Entry ID: 9260793). How to update the firmware of modules in general is described in detail in the STEP 7 Online Help under the topic of "Firmware Update".

The following requirements must be met:
 

No. Requirements
1 The ET 200S 1SI must be reachable online from the PG/PC.
2 The SI module must be slotted in a station with a header module IM151-1 standard (6ES7 151-1AA04-0AB0) or IM151-1 HF (6ES7 151-1BA01-0AB0).
  • You must operate the PROFIBUS either in DP V1 mode or
  • if you operate the PROFIBUS in DP V0 mode, the PG must be connected directly to it.
3 The files with the new vision of the firmware must be available in the file system of your PG/PC.
4 STEP 7 V5.1 SP3 or new

Tip:
If when using the menu command "PLC > Update Firmware", the current firmware version of the module is not recognized or displayed, then the requirements for an update are not fulfilled.

Keywords:
PtP, Technology modules


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.