×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 22180793, Entry date: 02/03/2015
(4)
Rate

Determining the transmission time for typical configurations on Industrial Ethernet

  • Entry
  • Associated product(s)
Task Automation projects often require intensive data exchange between SIMATIC S7 controllers. The possible communication paths vary considerably. These measurements allow you to estimate the transfer times for your case.

Task
Automation projects often require intensive data exchange between SIMATIC S7 controllers. The possible communication paths vary considerably. Numerous S7 controllers and S7 communication modules are available.

To be able to make the right selection in the concept phase of an automation project, it is important to know the communication performance of the planned configuration.

Important questions in this context are listed below:

  • Which S7 components are best suited for the planned automation project?
  • Which data transfer times are expected for typical configurations?
  • How does the data communication affect the cycle (OB1) of an S7 controller?
  • Which communications services can be used for specific S7 components?
  • Which communication service should be used considering performance aspects?

The following screen shows the schematic layout on a variant:



Fig. 1


Solution
To answer the above questions, Industry Automation and Customer Services carried out extensive measurements on typical configurations with SIMATIC components, which provide planning certainty for your plants:

  • Typical S7 controllers transmit data to up to 30 S7 controllers
  • Security configurations
  • Load programs with practical relevance in the corresponding S7 controllers enable values under real conditions

To correctly interpret the measured values, we recommend referring to the boundary conditions of the measurement in the documentation.

Overview of the measured variables  

Measured variable

Description

Transmission time Time from send trigger command to reception of the data in the respective data block of the receiver.
Cycle time sender Time between two process image transfers in the S7 controller of the sender.
Cycle time receiver Time between two process image transfers in the S7 controller of the receiver.
CbA transmission interval Time between two CbA transmission intervals for cyclic transmission (set in SIMATIC iMAP)
PNIO update time Time between two IO cycles of the IO controller. (calculated by STEP 7)

Note
Measurement was performed for some typical configurations. This does not mean that every possible configuration has been measured.

Measured values
We provide the results of the measurements as download in Excel format.

VersionMeasurement timeMeasured componentsDocumentation on measurementLink to Web GUIMeasurement values (Excel)
V 6.02019   components_list_V6 available soon Registrierung notwendig  IE_Comm-Measurements.xlsm
V 5.02018   components_list_V5 (708,5 KB)
CommIE_V5 
V 4.02009  components_list_V4 CommIE_V4 
V 3.02008  components_list_V3 CommIE_V3 
V 2.02007  components_list_V2 CommIE_V2 
V 1.02005  components_list_V1 CommIE_V1 


Last modification
Reactivation of Web Application 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.