×
Siemens Industry Online Support
Siemens AG
Тип сообщения: Сообщение о продукте ID сообщения: 22232975, Дата сообщения: 17.11.2005
(1)
Оценить

Release for general availability for SinuCom startup and service tools, Software Version 7.1 (V07.01.00)

  • Сообщение
  • Относится к продукту(ам)



With immediate effect, the startup and service tools
      SINUMERIK SinuCom NC, SinuCom ARC, SinuCom FFS,
      SinuCom PCIN and the startup tool; 
      Software Version 7.1

have been released for general availability. Software Version 7.1 replaces Software Version 6.4.





1. Overview:

The SINUMERIK 810D/840Di/840D/840D sl can be conveniently commissioned and serviced using the SinuCom startup and service tools which have been developed for OEM staff.

2. Functional extensions and improvements as compared to SinuCom Version V06.04.05 and startup tool V06.04.18
See also !21336365! and 19128867

 

SinuCom NC:
The support for Sinumerik startup has been extended to include the new control system generation Sinumerik solution line.
The following extensions are included:

-

Connection Wizard:
This Wizard configures the interface between PC/PG and target control system to be addressed via several query steps
(MPI interface for powerline, Ethernet interfaces for solution line). To ensure fast access, the control systems configured once can be stored as favorites.

-

Options Dialog:
The options dialog known from the SINUMERIK 840Di can also be used to select the options and enter the License key for the Sinumerik solution line control systems.

-

PROFIBUS Configuration:
The addresses defined can be assigned to the drive setpoints and actual values via the PROFIBUS configuration dialog.

-

Setpoint / Actual-Value Assignment:
The relevant drive setpoint/actual value can be assigned to the NC axis via the setpoint/actual-value assignment dialog.

 

 

SinuCom NCSI:
Supplementary condition:
No Safety Integrated acceptance test can be performed in Version 07.01.00. Remedy: Use V06.04.05.

 

 

SinuCom NCTRACE:

-

The Trace functions now also apply to the Sinumerik solution line control systems

 

 

SinuCom FFS:

-

Remains unchanged as compared with SinuCom 06.04.05

 

 

SinuCom ARC:

 

Remains unchanged as compared with SinuCom 06.04.05

 

 

SinuCom PCIN:

 

Remains unchanged as compared with SinuCom 06.04.05

 

 

SIMODRIVE 611digital/SINAMIC S120 startup tool:

 -

Extended by:
Operation on NCU 7x0 with Sinamics drives

 -

Now also includes:
Startup of Sinamics drives

-

SINUMERIK 840D sl license handling newly introduced


3. Prerequisites:
  

Tool

WIN 95

WIN 98

WIN ME

WIN 2000

WIN NT

WIN XP

SinuCom NC

-

-

-

-

-

Yes

SinuCom FFS

-

-

-

-

Yes

Yes

SinuCom ARC

-

-

Yes

Yes

Yes

Yes

SinuCom PCIN

Yes

Yes

Yes

Yes

Yes

Yes

Startup tool

-

-

-

-

-

Yes

 

"-"

Not supported

  

SinuCom NC:

-

Windows XP Prof. SP1 or SP2

-

Can be installed on PC/PG (alternatively on SINUMERK PCU 50/70 with HMI Adv.)

-

Minimum hardware requirements: Pentium III with 566 MHz; 256 MB RAM

-

SinuCom NC occupies approx. 7 MB of the Windows directory and 50 MB of the SinuCom NC directory

-

Recommended display resolution >= 800 x 600

-

NCU system software 05.01.22 (or later); recommended: >= 5.3

-

HMI Advanced 07.01.00.00 plus Hotfix 07.01.00.01

SinuCom NCTrace:

-
-

NCU software 05.03.37 or later (for IPO signals only)
NCU software 06.04.15 or later (for all functions)

-

HMI Advanced resp. HMI Base Software Version 6.3 (06.03.15 or later) and Software Version 6.4 (06.04.18 or later)

SinuCom NCSI (acceptance test):

-

with SinuCom NC 6.4:

 

+

NCU Software Version 6.4 (06.04.15 or later)

 

+

HMI Advanced resp. HMI Base Software Version 6.3 (06.03.15 or later) and Software Version 6.4 (06.04.18 or later)

 

+

Display resolution >= 800 x 600 and 640 x 480 (for OP 010; with scroll bar)

-

with SinuCom NC 7.1

 

+

No Safety Integrated acceptance test can be performed with Version 07.01.00.

SinuCom FFS, SinuCom ARC and SinuCom PCIN:

-

See the corresponding Readme file (*.txt)

SIMODRIVE 611digital/SINAMIC S120 startup tool:

-

The startup tool V07.01 can be combined with NCU 710/720 SW1.3 and 810D/840D Software Version SW6.x or later

-

The help system is based on the documentation for NCU SW1.3 (solution line) resp. NCU SW 7.2 (powerline)

-

The NC alarm texts are based on NCU-SW1.3 (solution line) resp. NCU-SW 7.2 (powerline)

-

The startup tool N07.01 can only run on Win XP

-

The startup tool N07.01 only supports the "new design"

-

The simulation is based on the 840D-NCU software 06.05.27 (NCK 51.13)

-

The "upgrade archive" function is not available for solution line

-

The startup tool V07.01 no longer supports V24 data transfer


4. Ordering data:
 

MLFB

Sales text





6FC5250-7AY00-1AG0
6FC5250-7AY00-1AG3

SINUMERIK 810D / 840DI SL /
840D / 840D SL; SINUCOM
STARTUP / SERVICE TOOLS
ON CD-ROM; SOFTWARE VERSION 7.1
           Single license, on CD-ROM
           Update/upgrade, on CD-ROM

 

The CD-ROM includes the following:

-

SinuCom NC

(ge/en/fr/it/sp)

V07.01.01

 

     with  CT editor
              HMI Base
              HMI Base
              

V01.00.00
V07.10.17
-
 

-

SinuCom ARC

(ge/en)

V01.02.04

-

SinuCom FFS

(ge/en)

V01.01.01

-

SinuCom PCIN

(en)

V01.03.03

-

Startup tool
     with  MPI driver
           HMI hotfix

 (ge/en/fr/it/sp/Simplified Chinese)

V07.10.17
V06.03.00.00

V07.01.00.01

-

 Installdisk.exe

 

V00.05.00.00

 

 

 

 

-

System Description08/2005 Edition
SinuCom NC Startup/Service Tool (en)

 



6FC5250-0AY00-0AG1
6FC5250-0AY00-0AG2

SINUCOM
STARTUP /SERVICE TOOLS
       Copy license
       Software Update Service

Further software versions:
SinuCom NC Software Version 6.2  6FC5250-6AY00-2AG0/3 is still available.
SinuCom NC Software Version 6.3  6FC5250-6AY00-3AG0/3 will be replaced by Software Version 6.4.
SinuCom NC Software Version 6.4  6FC5250-6AY00-4AG0/3 is still available.
Customers ordering the current Software Version 6FC5250-0AY00-0AG0 will receive Software Version 7.1. 


5. Documentation:
 

-

The documentation on SinuCom NC in English is available on CD-ROM and as online help.
Documentation in German (not available at the editorial deadline of the CD):
INC_0805_00.pdf ( 954 KB )

-

The documentation will be included as a separate document on the next DOConCD:
     SINUMERIK 840D sl/840D/840Di/810D 
     SINUMERIK SinuCom NC Startup Tool (INC).


6. Notes on "Cardware":

see 21336365



For more detailed information, please contact your local Siemens office.



Указания по безопасности
Для обеспечения и дальнейшего поддержания кибер-безопасности технической инфраструктуры, систем, машин и сетей необходимо внедрить комплексную концепцию информационной безопасности, которая соответствует последним достижениям науки и техники. Продукты и решения Сименс являются всего лишь одним из компонентов такой концепции. Более подробную информацию о кибер-безопасности можно получить здесь
https://www.siemens.com/cybersecurity#Ouraspiration.
Оценить сообщение
без оценки
Вопросы и обратная связь
Что вы хотите сделать?
Примечание: отзыв всегда относится к текущей статье / текущему продукту. Ваше сообщение будет перенаправлено техническим редакторам службы онлайн-поддержки. В течение нескольких дней вы получите ответ, если ваш отзыв содержит вопрос. Если у нас не возникнут вопросы по вашему отзыву, мы не будем вас беспокоить.
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
Отобразить эту страницу в новом дизайне
Панель управления mySupport