×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22279833, Entry date: 09/25/2014
(0)
Rate

MICROMASTER 4 (AOP): Message "No Drive Responding"

  • Entry
  • Associated product(s)
This FAQ applies only to the MICROMASTER 4 Advanced Operator Panel (AOP).

What is the cause of the AOP message "No Drive Responding"?

This means the AOP is attempting to connect to the drive, but it is not responding to the USS commands.
Pressing P twice will quit the error. The user should confirm that the communication baud rate set on the inverter is the same as that which is set on the AOP. Inverter parameter P2010 index 1 should be set to 6 which is 9600 baud.
To access the AOP's internal parameter set, the following procedure must be performed:

  1. Set mode to "Internal"
  2. Select "Parameters"
  3. Select the AOP Parameter Set
  4. View "All" parameters
  5. parameterization as follows:
    P0003 = 3
    P8552 = 0    Base Slave Address
    P8553 = 6    Default Baudrate
    P8554 = 0    Autobaud

Information

  • Description and further information you find in the AOP Operating Instructions; Entry-ID: 24532563
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.