×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22283667, Entry date: 10/23/2014
(1)
Rate

MICROMASTER 4 (MM4): Downloading a parameter set from an existing STARTER project

  • Entry
  • Associated product(s)
Applies to MICROMASTER 4
Why is there a problem when downloading a parameter set from an existing STARTER project into a new one with different inverter Firmware Version?

The firmware version of inverter and STARTER project needs to be the same.
You can see firmware version in parameter r18.

Steps to upgrade firmware version in STARTER project:

  1. Highlight the inverter in the project tree, clicking “ right mouse key”
  2. The pull down menu will give you the option “Target device”
  3. The pull down menu will give you the option “Upgrade device version / characteristic”
  4. Click on “Device version”
  5. Select the new Device Version
  6. Click on “Upgrade”

The STARTER projct will no upgrade to the selected firmware version.


Further information

  Uploading and downloading drive parameters of a MICROMASTER 4xx using STARTER (1,5 MB) 

Commissioning the inverter with STARTER ID: 31399077