×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 22309811, Entry date: 11/18/2005
(0)
Rate

Using PCS 7/TM-EA with PCS 7 H and F systems

  • Entry
  • Associated product(s)

QUESTION:
Can PCS 7/TM-EA be used with H and F systems of PCS 7?

ANSWER:
Following configurations have to be distinguished:

  • singular H or F CPU
    PCS 7/TM-EA can be used with a singular H and F CPU without problems.
     
  • redundant H or F CPUs in one rack
    Using PCS 7/TM-EA with redundant H and F CPUs in the same rack is not possible, as no switching of the Teleperm M I/O bus has been realized.
     
  • redundant H or F CPUs in separate cabinets
    It looks differently for redundant H and F CPUs which were not installed in the same rack but in separate cabinets, i.e. with separated I/O peripherals.
    This configuration has not been tested and released.
    If this configuration shall be used please ask the Technical Support.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.